Arduino Projects
  • Products & Partners
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog Sabertooth Dual Motor Driver
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Hallowed31
  • Date Created: 13 Aug 2024 1:56 AM Date Created
  • Views 1298 views
  • Likes 5 likes
  • Comments 0 comments
Related
Recommended

Sabertooth Dual Motor Driver

Hallowed31
Hallowed31
13 Aug 2024

This is code I cooked up in the Arduino Forum a few days ago to help someone who wanted to hack their kid's Powerwheels/Peg Perego 2WD ride on toy using a Sabertooth 2x60 motor controller. 

I was never happy with Dimension Engineering example sketch as they never really did what I wanted to do (which was this - I made an RC version a few years ago).

Be sure to read the sketch carefully, safety warning there, and there are options you may need to work though, plus all the connections are in the sketch.

/*********** Powerwheels Sabertooth *********************

    !!!!!!!!!!!!!!!  IMPORTANT  !!!!!!!!!!!!!!!
    !!!!!!!!!!!!!!!  IMPORTANT  !!!!!!!!!!!!!!!
    !!!!!!!!!!!!!!!  IMPORTANT  !!!!!!!!!!!!!!!

  THIS CODE WILL ALLOW OVERRIDING OF KID'S RIDE ON TOYS
  SUCH AS THOSE MADE BY POWERWHEELS AND PEG PEREGO

  IT IS UNTESTED CODE IN ACTUAL RIDE ON WITH RIDER.
      USE AT YOUR OWN RISK!
  DO NOT, I MEAN DO NOT USE ON RIDE ON TOY WITH ANY
  RIDER UNTIL IT HAS BEEN CALIBRATED AND THOROUGHLY
  TESTED TO THE SATISFACTION OF A COMPETENT ADULT
  CARE PROVIDER FOR THE RIDER IF THE RIDER IS NOT AN
  ADULT.

  THIS CODE CONTAINS NO EMERGENCY OVERRIDE AND THE TOY
  SHOULD ONLY BE OPERATED WITHIN THE REACH OF A
  COMPETENT ADULT CARE PROVIDER WHERE A MECHANICALLY
  OPERATED EMERGENCY STOP OVERRIDE DEVICE HAS BEEN INSTALLED,
  EFFECTIVELY REMOVING ALL BATTERY POWER TO THE MOTORS.

  END OF IMPORTANT NOTE

   ---------  INSTRUCTIONS TO BUILDER  ------------
        Requires changes to code depending on your hardware
        if using two position button type pedal, activate
        the line
        pinMode(sensorPin, INPUT_PULLUP);
        by uncommenting it.
        if using typical potentiometer, leave that line
        commented out.

        Also, in function void checkSpeedPot(){}
        have a read through and there's some stuff to set there
        Defaults to testing (printing data to PC over Serial)
        and assumes pushbutton type "all-or-nothing"
        throttle input. These can be adjusted according to
        the notes above and the comments found throughout
        this sketch.

        Also, select the instance of Sabertooth class that suits you
        (default is for Arduino Mega or other with Serial1 UART)

  The circuit:
  - potentiomenter to analog input 0
  OR if you use a switch type pedal
  - switch pin A0 to GND
  - forward switch to D3
  - reverse switch to D4
  - LED on digital pin 13 to ground
  - view values in Serial monitor, 9600 baud
  - Arduino TX to Sabertooth S1 (Uno) if selected
  - Arduino RX to Sabertooth S2 (Uno) if selected
    DEFAULT:
  - Arduino TX1 to Sabertooth S1 (Mega)
  - Arduino RX1 to Sabertooth S2 (Mega)

  Tested with 2 x Razor E300 scooter brushed motors @12V, no load
  and seems to be working as expected.
  Test motor specs:
  MY1016-B 24V 350W 2750 RPM electric scooter motor

  Sabertooth DIP switch settings for this Packetized Serial Mode:
   - 1: D for Packetized Serial address 128
   - 2: D
   - 3: D for LiPo, U for all other chemistries (battery cutoff switch)
   - 4: U for 9600 baud, reverse this for 19200 baud: baud select pin 1 U for autobaud
   - 5: U for 9600 baud, reverse this for 19200 baud: baud select pin 2
   - 6: U for Standard Simplified Serial

  by Hallowed31
  2024-07-27

  Library copyright Dimension Engineering, 2012
    "Copyright (c) 2012 Dimension Engineering LLC
    See license.txt for license details."
*/



#include <Sabertooth.h>

/* choose your version, normal or Mega. Use one only.
  (or roll your own changing 2nd argument in the Sabertooth instance) */

// use line below for Uno Serial on pins 0 and 1
//Sabertooth ST = Sabertooth(128); // address 128

// use line below for Mega, Leonardo, any with a Serial1
Sabertooth ST = Sabertooth(128, Serial1); // address 128, port Serial1

#define PUSHED LOW
#define RELEASED HIGH

const int maximum = 1017;
const int minimum = 13;
const byte speedPot = A0;
const byte heartbeatLED = 13;
//Hardware Serial connected to 1;
const byte backwardSwitch = 3;
const byte forwardSwitch = 4;

//10 * 50ms = 500ms (1/2 second) before a change is validated
const byte debounceAmount = 10;

//when counters reach 10 (i.e. 10 read cycles) we assumed a valid switch change
byte forwardCounter = 0;
byte backwardCounter = 0;

byte lastForwardSwitch = RELEASED;
byte lastBackwardSwitch = RELEASED;

enum { REVERSE = -1,
       NEUTRAL = 0,
       FORWARD = 1
     };

int directionFlag = NEUTRAL;
int speed = 0;
int m1 = 0; // signal to motor 1
int m2 = 0; // signal to motor 2

unsigned long heartbeatTime;
unsigned long checkSwitchesTime;
unsigned long checkSSpeedPotTime;

void setup() {
  Serial.begin(9600);
  Serial1.begin(9600); // if you got a compile error here, you don't have one of these
  SabertoothTXPinSerial.begin(9600);
  Sabertooth::autobaud(SabertoothTXPinSerial);
  // the line below is for a button type pedal
  // comment this out if using potentiometer
  pinMode(speedPot, INPUT_PULLUP);
  pinMode(forwardSwitch, INPUT_PULLUP);
  pinMode(backwardSwitch, INPUT_PULLUP);
  pinMode(heartbeatLED, OUTPUT);
}

void loop() {
  if (millis() - heartbeatTime >= 500ul) { //500ms
    heartbeatTime = millis();
    digitalWrite(heartbeatLED, !digitalRead(heartbeatLED));
  }

  if (millis() - checkSwitchesTime >= 50ul) { //50ms
    checkSwitchesTime = millis();
    checkSwitches();
  }

  if (millis() - checkSSpeedPotTime >= 100ul) { //100ms
    checkSSpeedPotTime = millis();
    checkSpeedPot();
  }

  /************************************************
    Other non blocking code goes here.
    That means no while(), no delay();
  *************************************************/

}

void checkSwitches() {
  // forward switch
  byte state;
  state = digitalRead(forwardSwitch);
  if (lastForwardSwitch != state) {
    forwardCounter++;
    if (forwardCounter >= debounceAmount) {
      //get ready for the next cycle
      forwardCounter = 0;
      lastForwardSwitch = state;
      if (state == PUSHED) {
        directionFlag = FORWARD;
      }
      else {
        directionFlag = NEUTRAL;
      }
    }
  }
  else {
    forwardCounter = 0;
  }

  // backward switch
  state = digitalRead(backwardSwitch);
  if (lastBackwardSwitch != state) {
    backwardCounter++;
    if (backwardCounter >= debounceAmount) {
      backwardCounter = 0;
      lastBackwardSwitch = state;
      if (state == PUSHED) {
        directionFlag = REVERSE;
      }
      else {
        directionFlag = NEUTRAL;
      }
    }
  }
  else {
    backwardCounter = 0;
  }
}

void checkSpeedPot() {
  speed = analogRead(speedPot);

  // uncomment for testing, comment out for final install
  // printRawData();

  /* IMPORTANT - use only ONE of these speed = map(etc) functions at at time */
  // for potentiometer type throttle
  // speed = (map(speed, minimum, maximum, 0, 1023)) / 8;  //for speed 0 to ±127

  // for pushbutton type throttle, map is reversed because INPUT_PULLUP
  speed = (map(speed, minimum, maximum, 1023, 0)) / 8;  //for speed 0 to ±127

  // uncomment for testing, comment out for final install
  //  printMappedData();
  speed = constrain(speed, 0, 127);  //for speed 0 to ±127
  speed = directionFlag * speed;
  m1 = speed;
  m2 = speed;
  // uncomment for testing, comment out for final install
  // printFinalDriveSignal();

  ST.motor(1, m1); // motor 1, speed cast to m1
  ST.motor(2, m2); // notor 2, speed cast to m2
}

void printRawData() {
  Serial.print("Throttle Input: ");
  Serial.print(speed);
  Serial.print(" ");
}
void printMappedData() {
  Serial.print("Throttle Mapped To: ");
  Serial.print(speed);
  Serial.print(" ");
}
void printFinalDriveSignal() {
  Serial.print("  Final Drive Signal M1: ");
  Serial.print(m1);
  Serial.print("  Final Drive Signal M2: ");
  Serial.println(m2);
  Serial.println();
}