Arduino
  • Products & Partners
  • More
Arduino
Blog An Arduino/Raspberry Pi Based Wireless Light Harness
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: screamingtiger
  • Date Created: 11 Jun 2015 1:17 PM Date Created
  • Views 7903 views
  • Likes 3 likes
  • Comments 76 comments
  • wirless_trailer
Related
Recommended

An Arduino/Raspberry Pi Based Wireless Light Harness

screamingtiger
screamingtiger
11 Jun 2015

I am going do this small side project as a way to take a break from my main project.  For a basic introduction please see my original blog post at http://www.element14.com/community/people/screamingtiger/blog/2015/04/20/a-small-project-idea--wireless-trailer-lighting-control

 

If anyone has concerns about my project, please post them in that thread.  I have changed the design slightly after doing  some research and testing.  I am also going to have a control panel in the car with me so I can monitor things as well as manually test the lights.

 

The car has running lights, brake lights, and turn signals all on separate channels.  However the trailer lights only have 2 channels as the running lights also function as turn signals. My initial analysis was incorrect that the running lights also function as brake lights.

 

First a tentative parts list and then I will explain.

2X Arduino mini pros 16mhz boot loader

1X Raspberry Pi model B

1X 2.5" TFT touchscreen LCD

1X 4 channel mechanical relay

6X AMS1117 SO-223 5V regulators

3X NRF24L01+ wireless transceivers

1X 1.5 watt solar charger

3X enclosures

1X 20,000mAh (20Ah) 12V lead acid battery

1X hobbyking 5V/5A regulator

1X 1000 mAh 2s LIPO

 

Explanation of parts :

There are 3 units involved. We have the unit that reads the car's lights, the unit that controls the trailer lights, and the unit that acts as a control panel.  All 3 are connected via the wireless adapters.

 

2X Arduino mini pros 16mhz boot loader

These will be used for the units that read the lights and control the trailer lights.  I have some of these on hand is why I went with them and the small footprint will allow me to tuck it away nicely.

 

1X Raspberry Pi model B and 1X 2.5" TFT touchscreen LCD

This will function as the main control panel with a simple interface.  The Pi attaches easily to the LCD which is why I chose this route.  Its way overkill but I feel it will be useful for other projects that also need a remote or control panel.  The control panel will allow monitoring as well as manual control of the lights for testing.

 

1X 4 channel mechanical relay

The stock lights on my trailer pull 2A for the brakes lights per side, and 500 mA per side for the running lights.  Originally I was going to use a mosfet but I see no reason with this high of current.  The brake lights will be turned on at the same time so the relay will see 4A.  However the running lights will be on separate channels as they also function as blinkers.  The 4th channel I may use to turn on internal lights in the trailer remotely.

 

6X AMS1117 SO-223 5V regulators

These small regulators will be used to power the Arduinos off of the main 12V sources which come from the vehicle as well as the 12V battery in the trailer.  They are also used to read the  vehicle lights.  My plan is to splice into the lines of each light the same way I did before when installing an off the shelf light controller.  The lights will be routed to the 5v regulators which then step down the voltages to 5V for reading via the GPIO pins on the Arduino.  I will need 4 regulators to read the lights.  1 for the brake lights, 1 for the running lights, and 1 each for each turn signal.

 

3X NRF24L01+ wireless transceivers

These 2.4ghz transceivers are similar to an I2C connection and a serial connection combined.  Each one has an ID and you can broadcast information. I will have a small protocol in place for error correction as well as some minor tamper proofing.  I don't want a rogue 2.4ghz signal to be able to mess with my lights.  I will be using a command set that requires a sequence of bytes in order to validate commands.

 

1X 1.5 watt solar charger

These can be had from Harbor Freight and low cost.  I decided that the trailer might as well be "green" and charge its own battery.  Besides its just another thing for me to forget to do.

 

The rest of the items are self explanatory and used to house the items and power the Pi.

 

I may choose to get some LED based trailer lights, but I am going to stick with the stock trailer lights for now until I have a working project.

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago in reply to screamingtiger +3
    Joey Did you remove the jumper .. JD-VCC to VCC ? You apply the 12v to JD-VCC NOT THE VCC PIN The 5v on the VCC pin is to power the Optocouplers ... Also note that these turn on with a LOW so you need…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to screamingtiger +2
    80mA for Arduino and 1A for lights adds up to 1.08Amps, not 1.8. This would provide a much longer life time (18.5 Hrs) so even with brakes you should easily get 10-12 Hr (Unless you're a heavy breaker…
  • clem57
    clem57 over 11 years ago +2
    Totally amazed is the word today. Plus a tropical depression has taken over here. LOL
  • screamingtiger
    screamingtiger over 11 years ago

    Well I set aside this evening to work and my soldering iron DIED.  All I had was a big butane powered soldering iron, that is actually meant to be a butane torch.  So my solder is not perfect but its not worse than the Chinese nrf24lr01 stuff I am using.

     

    This is the unit that connects to the car.  The wires coming out (under my fingers) attach to the input side of the 5V regulators, and the arduino reads the output from the regulator.  These wires will connect to a plug that connects to my lights which is already wired.  The current draw should be in micro amps so I hope it is enough to turn on the regulator.  Thoughts?

     

    The wireless adapter is connected to the arduino as well.

     

    All I am missing is my 3.3V regulators which will be here tomorrow.  The wireless adapter needs 3.3.

     

    Question: EDIT:  Answered my own question, I have added a 5V regulator for the arduino to run off of too.

    I am open to criticism, I do not have fancy tools yet to build things.  This is the 2nd "circuit" I have ever made.  This is a 20 cent perf board and it is very low quality.  The main pads on the end are not connected to the underneath pads.  I hate that.

     

    image

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to screamingtiger

    We did a session on wireless charging.

    It requires a maximum 10mm gap, but is not exactly connected ...

     

    can't see why volts from the vehicle is a problem.

    I like the wireless connection to keep the trailer away from your vehicle wiring, but power is power and a fuse stops the shorts from causing harm.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to screamingtiger

    How did you know where I live?

    smile you're looking worried.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to mcb1

    I have a fused wire running form the battery to the back of the vehicle from a previous trailer light harness, I will be using that.  I do not care to power the trailer from the vehicle as the defeats the purpose unless you guys have an idea of how I can transmit power!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to mcb1

    Mark you are SCARY  image  The first set of lights was $22 USD and within 100 miles of my location!  I ordered it on the spot, if the ship tomorrow it should get here by Friday easily.

     

     

    How did you know where I live?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>