Arduino
  • Products & Partners
  • More
Arduino
Blog Arduino | 3 New MKR Shields for Your "IoT: In the Cloud" Projects: Arduino MKR RGB, MKR ENV, and MKR THERM!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 18 Apr 2019 5:37 PM Date Created
  • Views 4942 views
  • Likes 11 likes
  • Comments 18 comments
  • arduino mkr therm
  • arduino mkr env
  • mkr_shields
  • arduino mkr rgb
  • exclusive_mkr_shields
Related
Recommended

Arduino | 3 New MKR Shields for Your "IoT: In the Cloud" Projects: Arduino MKR RGB, MKR ENV, and MKR THERM!

tariq.ahmad
tariq.ahmad
18 Apr 2019
image

Arduino Home

An Open-Source platform to create digital devices and interactive objects that sense and control physical devices.

Arduino Tutorials
Arduino Projects

 

In the comments below:  Let Us Know How You Would Use the MKR RGB, MKR ENV, and MKR Shield in Your Arduino Projects!

 

Submit a Project Proposal for an IoT: In the Cloud project and we'll send out a limited number of shields for projects that use them!

 

View tech specs and unboxing videos for the Arduino MKR RGB, MKR ENV, MKR THERM shields. Datasheets and Eagle Files are also attached below.

 

There's still time left for your  IoT: In the Cloud project.   This year for Arduino Day we challenged you to do Arduino Projects for Arduino Day 2019:  Arduino MKR Projects in the Cloud!

 

Recently, these new shields were launched exclusively through Farnell.  This will give you a chance to use the new shields in your IoT projects or any Arduino projects you are working on.  If you have an idea for an IoT: In the Cloud project that uses one of the shields, we'll send you one of the new shields to help you complete your project.   The competition closes on May 14th and you can read details at:  Project14 | IoT in the Cloud: Make Use of a Wireless Technology and a Cloud Provider!

 

Below are some specs and unboxing videos for the 3 new shields from Arduino!

 

ARDUINO MKR RGB SHIELDARDUINO MKR ENV SHIELD
imageimage
Buy NowBuy NowBuy NowBuy Now

Write messages and add graphics with this shield.

 

A ready to use library with examples and methods is available for use to easily write static and scrollable text.

 

You can use this shield to show values from your board and is controllable from the Arduino IoT cloud. No need of solder, or special adapters, just plug the RGB matrix shield on top of your favourite MKR board and you are ready to go!

 

The mounted LED's are very dense and bright, with full RGB colours!

The MKR ENV Shield allows a MKR board to acquire environmental data collected by an array of sensors.

 

These sensors are of the latest generation and measure:

  • Atmospheric pressure
  • Temperature and humidity
  • Ultraviolet UVA intensity Ultraviolet UVB intensity
  • UV Index (calculated)
  • Light intensity (in LUX)

 

To help you build projects and store the data collected locally, this shield has a slot for a microSD card (not provided).

 

There is a ready to use library with examples and methods to read values from the different sensors, that provides an easy and smooth integration path.

 

Sensors used :

  • ST LPS22HB :  atmospheric pressure
  • ST HTS221HTS221  : temperature and humidity
  • VISHAY TEMT6000 : Lux of the ambient.
  • VISHAY VEML6075VEML6075 : UltraViolet wavelengths  A / B
LEDs84  RGB APA102
Input Voltage5V
Operating Voltage3.3V
Maximum Current2.5A
CommunicationSPI
Length61.5 mm
Width27 mm
Weight32 gr.
ICs

LPS22HB

TEMT6000

VEML6075VEML6075

Input Voltage3.3V
Operating Voltage3.3V
Ranges

Pressure: 260 to 1260 hPa

rH sensitivity: 0.004% rH/LSB

Humidity accuracy: ± 3.5% rH, 20 to +80% rH

UVA, UVB and UVBI measurment

CommunicationI2C/Analog
Length61 mm
Width25 mm
Weight32 gr.
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
ARDUINO MKR THERM SHIELD
image
Buy NowBuy Now

The MKR THERM Shield allows a board of the MKR family to acquire temperatures from a thermocouple of type K and a DS18Bxx digital one wire sensor. The Thermocouple is a kind of temperature sensor that offers high accuracy and a wide range of measured temperatures. Its analog nature requires specific interfacing and this shield relies on the MAX31855 thermocouple digital interface.

 

The two connectors of the MKR THERM Shield allow the usage of Type K thermocouples with or without a plug attached to the metal wires.

 

The MKR THERM Shield has its own library to read the temperature measured by the thermocouple

ConnectorsK TYPE  DALLAS DS18S20  (to solder) Screw terminal block
Input Voltage3.3V
Operating Voltage3.3V
Operating Temperature-200°C + 700°C
CommunicationSPI/1Wire
ICMAX31855
Length61 mm
Width25 mm
Weight32 gr.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Arduino MKR Shields:

 

Product NameQuantity
Arduino MKR RGB Shield1Buy NowBuy Now
Arduino Environmental Shield1Buy NowBuy Now
Arduino MKR Thermal Shield1Buy NowBuy Now

 

 

In the comments below:  Let Us Know How You Would Use the MKR RGB, MKR ENV, and MKR THERM Shield in Your Arduino Projects!

 

Submit a Project Proposal for an IoT: In the Cloud project we'll send you a board for projects that use them!

Attachments:
imagedm00140895.pdf
imageveml6075.pdf
imageMKRENVShieldV4.0_sch.pdf
imageMKRRGBShieldV3.0_sch.pdf
imageMKRTHERMShieldV3.0_sch.pdf
imagehts221.pdf
imageMAX31855.pdf
MKRENVShield-reference.zip
MKRTHERMShield-reference.zip
  • Sign in to reply

Top Comments

  • ralphjy
    ralphjy over 7 years ago +5
    Nice additions. I could probably use a MKR THERM shield. Not sure why they put the stackable headers on the ENV shield. I doubt that you would want to obscure the sensors. It would be better if they provided…
  • neilk
    neilk over 7 years ago +4
    The ENV shield looks useful - measuring UVA, UVB and LUX could be an interesting extension to measuring temperature and moisture levels in a horticultural application Neil
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to jomoenginer +4
    I found a way to get the i2c working andkeep the wifi wofking. I posted it in one of the Project14 articles. I'll try to find it back ...
  • winzurf
    winzurf over 7 years ago

    I'm developing a satellite controlled solar powered FM radio station for use in remote locations. The MKR ENV Shield would be a great option for monitoring the environmental status and performance of the unit.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vimarsh_
    vimarsh_ over 7 years ago in reply to mahmood.hassan

    Yes,

    I was also thinking the same!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mahmood.hassan
    mahmood.hassan over 7 years ago

    I have already built a Energy Efficient Room Lighting system but now I am doing a comparison between normal lighting V EE lighting system with cloud data storage image

    ENV shield can be useful in it but I am not using Arduino MKR boards image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mahmood.hassan
    mahmood.hassan over 7 years ago

    These shields are looking awesome.

    TEMT6000 sensor doesn't give a stable value. You need to take average of multiple values for a stable value but on the other hand digital ALS gives much stable value.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mahmood.hassan
    mahmood.hassan over 7 years ago in reply to vimarsh_

    Yeah these two can be used together but If you place RGB shield over ENV shield then you will be blocking light and UV sensors or other way around it will be useless to place RGB shield beneath the ENV shield. Now the only option is to use jumper wires to connect one of these shields image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>