Arduino
  • Products & Partners
  • More
Arduino
Blog Long Range Sensor Array - Pi IoT  Blog 7
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 16 Nov 2016 7:19 AM Date Created
  • Views 1286 views
  • Likes 5 likes
  • Comments 2 comments
Related
Recommended

Long Range Sensor Array - Pi IoT  Blog 7

dougw
dougw
16 Nov 2016

This blog documents some belated progress on my Star Trek themed Pi IoT design challenge entry. It is being put in the arduino area since that is where it is most useful.

I wanted to make the subsystems useful and built well enough to work reliably in their target environment, so this sensor array is built using a custom PCB.

The PCB did not arrive until well after the challenge was over, but it worked perfectly with no errors when I assembled it.

The card features an arduino pro micro which has a couple of quirks to be aware of:

  1. Sketches can defeat the USB so to get back into programming mode, you need to push the reset button twice, which reactivates the USB for 8 seconds, hopefully allowing you to get your software load started.
  2. I used the 3.3V variant of the pro micro so it could directly connect to the Bluetooth module.  This cpu runs at 8 MHz so you need to be sure the compiler is aware of the clock frequency, or all communications timing will be messed up. I installed the pro micro board type in the arduino IDE using this instructional note:

Other features of the card include an HC05 Bluetooth module, a Nokia 5110 LCD, a DHT11/22 temperature/humidity sensor a power switch, a reset switch, a solar panel connector and battery connector a recharging circuit, an I2C connector, a couple of input connectors (analog or digital).

Since I had to order a batch of 10 (for $10) I designed the card to have a little more general capability than just a remote temperature sensor.

The card has extra connectors for more sensors, but the main addition is an LCD connector, allowing it to be used as a stand-alone weather station.

Here is a video showing the system in action:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The android app was developed using App Inventor 2 from MIT.

 

Links to the Pi IoT Design Challenge site:

Pi IoT

Pi IoT - Smarter Spaces with Raspberry Pi 3: About This Challenge

 

Links to blogs about the Star Trek IoT Alcove project:

Pi IoT - Star Trek IoT Alcove - Blog 1

element14 and the photon torpedo - Pi IoT Blog 2

How many tablets to use? Pi IoT Blog 3

Starship Enocean Voyager

The Starship Enocean Voyager - Pi IoT Blog 4

LCARS (Library Computer Access Retrieval System){Star Trek} - Pi IoT Blog 5

LCARS Tablets

Henrietta LCARS

Alcove Transporter

Henrietta LCARS - Pi Iot Blog 6

arduino bluetooth weather station

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 9 years ago +1
    Hi Doug, Nice presentation! Very cool that such a wireless weather station can be built for much less than the typical weather station from retailers (and yours has a far better local and remote display…
  • teprojects1
    teprojects1 over 9 years ago +1
    Hey Doug, Amazing presentation! I think your wireless weather station is cheaper then the retailer one, If you give a new look to this like hardware than it can be your new product which is ready to be…
  • teprojects1
    teprojects1 over 9 years ago

    Hey Doug,

     

    Amazing presentation! I think your wireless weather station is cheaper then the retailer one, If you give a new look to this like hardware than it can be your new product which is ready to be sale image what you said?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago

    Hi Doug,

     

    Nice presentation!

    Very cool that such a wireless weather station can be built for much less than the typical weather station from retailers (and yours has a far better local and remote display..).