Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum PIR
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 415 subscribers
  • Views 1398 views
  • Users 0 members are here
Related

PIR

lanzrye
lanzrye over 7 years ago

is it possible that the PIR motion sensor only detects a human only?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 7 years ago +4
    Hi Lanz, Unfortunately the design of the basic PIR can not discriminate between different heat sources. It reacts to changes in the heat signatures in the field of its view. If they are static it remains…
  • genebren
    genebren over 7 years ago +4
    Hi Lanz, Welcome to the element14 community. There have been a lot of conversation here on this same topic. Like jw0752 mentions above, PIR sensors in and of themselves do not discriminate the source of…
  • genebren
    genebren over 7 years ago in reply to jw0752 +4
    Another good point. On the same concept I referenced above (shuttering), we used notch filters on top of an array of PIR elements to narrow our view to certain areas of the IR spectrum (both long and short…
Parents
  • BigG
    BigG over 7 years ago

    Ok, sorry I couldn't resist being little facetious... as this was the first thing that popped into my head. As in, I very much doubt there is any sensor out there that can readily determine the genetic makeup of a human.

     

    So I assume you are asking whether a PIR can differentiate the heat signature of an adult human form (as in adult body mass walking upright) from something else. And the anwer is... sort of... as in, a pyroelectric sensor (PIR) also requires the right type of fresnel lens to help determine this. If you use a "curtain" type fresnel lens, which has a narrow vertical field of view combined with a wide horizontal field of view, this lens can be positioned in such a way as only detect objects of a certain height, for example. If you then combine this technique with filtering or the methods, as described above, then you have a good chance of differentiating. Another option to improve results, is to also use two PIRs at different heights, and use as a comparitor where both need to trigger concurrently, to derive that it is a human form being detected.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 7 years ago

    Ok, sorry I couldn't resist being little facetious... as this was the first thing that popped into my head. As in, I very much doubt there is any sensor out there that can readily determine the genetic makeup of a human.

     

    So I assume you are asking whether a PIR can differentiate the heat signature of an adult human form (as in adult body mass walking upright) from something else. And the anwer is... sort of... as in, a pyroelectric sensor (PIR) also requires the right type of fresnel lens to help determine this. If you use a "curtain" type fresnel lens, which has a narrow vertical field of view combined with a wide horizontal field of view, this lens can be positioned in such a way as only detect objects of a certain height, for example. If you then combine this technique with filtering or the methods, as described above, then you have a good chance of differentiating. Another option to improve results, is to also use two PIRs at different heights, and use as a comparitor where both need to trigger concurrently, to derive that it is a human form being detected.

    • Cancel
    • Vote Up +3 Vote Down