Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum PIR
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 415 subscribers
  • Views 1398 views
  • Users 0 members are here
Related

PIR

lanzrye
lanzrye over 7 years ago

is it possible that the PIR motion sensor only detects a human only?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 7 years ago +4
    Hi Lanz, Unfortunately the design of the basic PIR can not discriminate between different heat sources. It reacts to changes in the heat signatures in the field of its view. If they are static it remains…
  • genebren
    genebren over 7 years ago +4
    Hi Lanz, Welcome to the element14 community. There have been a lot of conversation here on this same topic. Like jw0752 mentions above, PIR sensors in and of themselves do not discriminate the source of…
  • genebren
    genebren over 7 years ago in reply to jw0752 +4
    Another good point. On the same concept I referenced above (shuttering), we used notch filters on top of an array of PIR elements to narrow our view to certain areas of the IR spectrum (both long and short…
Parents
  • dougw
    dougw over 7 years ago

    A simple PIR sensor cannot uniquely identify a human. A PIR sensor detects long wave infrared energy. Many things generate this type of energy. All warm-blooded animals and all sources of heat generate this type of energy. A human has a characteristic temperature that is different from most other emitters and humans have a defined size range that limits the set of possible sources, so a more complex PIR sensor that can measure temperature and size may be able to distinguish a human, but it would likely require a full thermal camera and significant image processing to get any kind of accuracy.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 7 years ago

    A simple PIR sensor cannot uniquely identify a human. A PIR sensor detects long wave infrared energy. Many things generate this type of energy. All warm-blooded animals and all sources of heat generate this type of energy. A human has a characteristic temperature that is different from most other emitters and humans have a defined size range that limits the set of possible sources, so a more complex PIR sensor that can measure temperature and size may be able to distinguish a human, but it would likely require a full thermal camera and significant image processing to get any kind of accuracy.

    • Cancel
    • Vote Up +3 Vote Down