Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum How do I connect Vcc or signal to multifunctional pin
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 416 subscribers
  • Views 1595 views
  • Users 0 members are here
Related

How do I connect Vcc or signal to multifunctional pin

SGarciaV
SGarciaV over 7 years ago

Hi all, I am working on this Arduino project which involves reading non-volatile memory. Since the design is to be compatible with memory chips of different sizes, I need to be able to configure the connections for each of these chips.

I have one pin in particular that for one chip is an address line (A13) and for another chip it is Vcc. Fr other pins, I can easily use a multiplexor to select the right signal that should go to the pin; however, I am wary about doing this for a Vccline sine this will need a higher current than the signal lines.

 

Specifically, I am looking at 32K x 8 and 2K x 8 chips. When placed in the socket, pin 26 (with respect to a 28 pin package) should be Vcc for the 2K chip or A13 for the 8K chip.

 

Any orientation is welcomed! Thank you, Saga

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 7 years ago +1
    I would suggest you build a logic table with all the examples you have. Then group common elements together. Take the most general cases and handle these first. Use the more specific ones or less general…
  • shabaz
    shabaz over 7 years ago +1
    Also, strongly suggest you read and experiment with transistors (BJT and MOSFETs), because sometimes the solutions with them are easy, for controlling power, which is what you're essentially trying to…
  • clem57
    clem57 over 7 years ago in reply to shabaz +1
    Thanks for the Links shabaz . And it works from a browser too.
  • clem57
    clem57 over 7 years ago

    I would suggest you build a logic table with all the examples you have. Then group common elements together. Take the most general cases and handle these first. Use the more specific ones or less general as hopefully one offs of the general case.As you go through this exercise, it becomes more obvious a simpler path to the design you will need.

    Just my thoughts,

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago

    Also, strongly suggest you read and experiment with transistors (BJT and MOSFETs), because sometimes the solutions with them are easy, for controlling power, which is what you're essentially trying to do. Schottky diodes can sometimes be helpful too, for reasons that can become clear once you're trying to connect one or more signals (or power sources) in an 'or' gate type solution. 

    If you need help with the experimentation, simulation is a good way forward too, e.g. falstad simulator: https://www.falstad.com/circuit/

    Example simulations (there are some with transistors there too, that you could play with or edit):  https://www.falstad.com/circuit/e-index.html

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to shabaz

    Thanks for the Links shabaz . And it works from a browser too.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • SGarciaV
    SGarciaV over 7 years ago

    Thank you both for your replies. I appreciate the links. The simulator is way cool!

     

    BB-Sphere, thanks for the helpful advice. In fact, this is what I did and managed to simplify most of the lines. I ended up with only one line needing to switch between a signal line and Vcc.

     

    Best regard to both, Sgarcia

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to SGarciaV

    Glad to help you. Could you please mark answer correct for others that may follow.

    Happy playing!

    Clem