Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum How do I connect Vcc or signal to multifunctional pin
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 416 subscribers
  • Views 1597 views
  • Users 0 members are here
Related

How do I connect Vcc or signal to multifunctional pin

SGarciaV
SGarciaV over 7 years ago

Hi all, I am working on this Arduino project which involves reading non-volatile memory. Since the design is to be compatible with memory chips of different sizes, I need to be able to configure the connections for each of these chips.

I have one pin in particular that for one chip is an address line (A13) and for another chip it is Vcc. Fr other pins, I can easily use a multiplexor to select the right signal that should go to the pin; however, I am wary about doing this for a Vccline sine this will need a higher current than the signal lines.

 

Specifically, I am looking at 32K x 8 and 2K x 8 chips. When placed in the socket, pin 26 (with respect to a 28 pin package) should be Vcc for the 2K chip or A13 for the 8K chip.

 

Any orientation is welcomed! Thank you, Saga

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 7 years ago +1
    I would suggest you build a logic table with all the examples you have. Then group common elements together. Take the most general cases and handle these first. Use the more specific ones or less general…
  • shabaz
    shabaz over 7 years ago +1
    Also, strongly suggest you read and experiment with transistors (BJT and MOSFETs), because sometimes the solutions with them are easy, for controlling power, which is what you're essentially trying to…
  • clem57
    clem57 over 7 years ago in reply to shabaz +1
    Thanks for the Links shabaz . And it works from a browser too.
Parents
  • SGarciaV
    SGarciaV over 7 years ago

    Thank you both for your replies. I appreciate the links. The simulator is way cool!

     

    BB-Sphere, thanks for the helpful advice. In fact, this is what I did and managed to simplify most of the lines. I ended up with only one line needing to switch between a signal line and Vcc.

     

    Best regard to both, Sgarcia

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • SGarciaV
    SGarciaV over 7 years ago

    Thank you both for your replies. I appreciate the links. The simulator is way cool!

     

    BB-Sphere, thanks for the helpful advice. In fact, this is what I did and managed to simplify most of the lines. I ended up with only one line needing to switch between a signal line and Vcc.

     

    Best regard to both, Sgarcia

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • clem57
    clem57 over 7 years ago in reply to SGarciaV

    Glad to help you. Could you please mark answer correct for others that may follow.

    Happy playing!

    Clem