Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Error message when trying to upload to Arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 416 subscribers
  • Views 839 views
  • Users 0 members are here
Related

Error message when trying to upload to Arduino

marktaylor
marktaylor over 6 years ago

So I am currently working with an arduino nano and I just built a prototype PCB for the system I was working with on a breadboard previously. After checking the PCB connection many times I finally tested it with my nano. Everything seems to be working as expected. However, now that I am further developing the sketch I want to run I cannot upload and am getting the error shown below. This error only occurs when seated in the headers on my PCB. If I take the nano off the board then everything is fine and I can upload my sketch. What are some potential issues with my PCB that could be causing this? Is it possible to answer this without seeing the board? Is it safe to keep using the PCB as is and just unseat the nano every time I want to update the sketch?

  • Sign in to reply
  • Cancel

Top Replies

  • Sean_Miller
    Sean_Miller over 6 years ago +2
    I can't see your error message for some reason, but I like a good challenge. :-) If you are confident on your solder joints and the design, you had no shorts when you tested the un-populated board, it…
  • aethertec
    aethertec over 6 years ago +2
    Well.. Your error message cannot be seen but lets try to figure this out anyway.. My broad guess is that you occupied the Rx Tx pins on your designed PCB for some different use. If you are sharing those…
Parents
  • Sean_Miller
    Sean_Miller over 6 years ago

    I can't see your error message for some reason, but I like a good challenge.  :-)

     

    If you are confident on your solder joints and the design, you had no shorts when you tested the un-populated board, it uploads with the board not installed, and the assembled project works within your expected amp range - you are good. If you don't know your amp draw, you should get one of these.

     

    I suspect you can't upload because your circuit is interfering with the serial pins or reset pin.  The original bootloader for the Nano (discussed here) gave an issue for analog pins as well.  So, you may want to check to see if you need to flash the bootloader

     

    I had trouble like this in my past with the ESP8266.  In turn, I put a tiny switch on my PCB that allowed me to switch it to "program" mode.  It was simply in line with the offending pin.

     

    To find the offending pin, I'd use jumper wire to land my headers.  Remove one at a time until you find the sucker.  Do a little dance when you do.

     

    See ya',

    Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Sean_Miller
    Sean_Miller over 6 years ago

    I can't see your error message for some reason, but I like a good challenge.  :-)

     

    If you are confident on your solder joints and the design, you had no shorts when you tested the un-populated board, it uploads with the board not installed, and the assembled project works within your expected amp range - you are good. If you don't know your amp draw, you should get one of these.

     

    I suspect you can't upload because your circuit is interfering with the serial pins or reset pin.  The original bootloader for the Nano (discussed here) gave an issue for analog pins as well.  So, you may want to check to see if you need to flash the bootloader

     

    I had trouble like this in my past with the ESP8266.  In turn, I put a tiny switch on my PCB that allowed me to switch it to "program" mode.  It was simply in line with the offending pin.

     

    To find the offending pin, I'd use jumper wire to land my headers.  Remove one at a time until you find the sucker.  Do a little dance when you do.

     

    See ya',

    Sean