Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum rectifier bridge
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 415 subscribers
  • Views 912 views
  • Users 0 members are here
Related

rectifier bridge

mfranklin
mfranklin over 6 years ago

Hello, I,m a first year electronic engineer from Jamaica. I am currently trying to make a 5v dc supply.

Going through my components I realised that I have 3 1n4004 diodes and 1 1n4007 diode. So I was wondering can a rectifier bridge be made from these diodes ?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 6 years ago +3
    Hi Maliek, The 1N4004 can handle up to 400 Volts and the 1N4007 can handle up to 1000 Volts. The transformer you will be using is certainly to be in the range of 16 volts or less (22 Volts Peak) to drive…
  • gadget.iom
    gadget.iom over 6 years ago +2
    You should be able to use that 1N4007 together with the 4004s without any issues at all.
  • colporteur
    colporteur over 6 years ago +1
    Look at the spec sheets for the diodes and the output should be kept to the lowest of the two devices. The diodes are capable of being a bridge rectifier just mixing an matching can cause issue as you…
Parents
  • jw0752
    jw0752 over 6 years ago

    Hi Maliek,

    The 1N4004 can handle up to 400 Volts and the 1N4007 can handle up to 1000 Volts. The transformer you will be using is certainly to be in the range of 16 volts or less (22 Volts Peak) to drive an LM7805 or equivalent regulator. As Paul and Sean indicated they will work just fine together for your application. If you want to experiment with something interesting check out making a MOSFET Bridge. It will eliminate most of the 1.4 Volt drop in a conventional bridge. I played with this a while back and here is my blog:

     

    https://www.element14.com/community/people/jw0752/blog/2017/02/01/exploring-the-lt4320-ideal-diode-bridge-controller

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 6 years ago

    Hi Maliek,

    The 1N4004 can handle up to 400 Volts and the 1N4007 can handle up to 1000 Volts. The transformer you will be using is certainly to be in the range of 16 volts or less (22 Volts Peak) to drive an LM7805 or equivalent regulator. As Paul and Sean indicated they will work just fine together for your application. If you want to experiment with something interesting check out making a MOSFET Bridge. It will eliminate most of the 1.4 Volt drop in a conventional bridge. I played with this a while back and here is my blog:

     

    https://www.element14.com/community/people/jw0752/blog/2017/02/01/exploring-the-lt4320-ideal-diode-bridge-controller

     

    John

    • Cancel
    • Vote Up +3 Vote Down