Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Powering Arduino with 5V pin and using USB for serial comms
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 414 subscribers
  • Views 9544 views
  • Users 0 members are here
Related

Powering Arduino with 5V pin and using USB for serial comms

Andrew J
Andrew J over 5 years ago

I Want to power a Nano or Mega with the 5V pin from my own regulated 5V supply.  But I also want to attach a USB cable for serial comms from a PC.  Looking at the schematic, there doesn’t appear to be any protection or mediation between the USB port and the 5V line only USB and Vin. 

I don’t need power from the USB port but I do need it to be recognised as a COM port on the PC.  Has anyone tried this?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 5 years ago +5
    Hi Andrew, I'm not super familiar with Arduino Nano/Mega, I took a look at the Nano schematic , and there is a diode between +5V and VUSB which should meet your need. I think the VIN supply won't interfere…
  • Andrew J
    Andrew J over 5 years ago in reply to shabaz +5
    I missed that on the Nano schematic - I looked at the PDF on the official site and the auto-selector circuit is tucked up at the top partially obscured by something else! But, yes that would give the protection…
  • Andrew J
    Andrew J over 5 years ago +4
    To wrap this up, I think the easiest thing to do is provide footprints for a USB-UART circuit so that if necessary I can bypass the USB power issue altogether! Something like a Microchip MCP2221a. I can…
  • shabaz
    shabaz over 5 years ago

    Hi Andrew,

     

    I'm not super familiar with Arduino Nano/Mega, I took a look at the Nano schematic, and there is a diode between +5V and VUSB which should meet your need.

    I think the VIN supply won't interfere with the ability to plug in via the USB. Everything on the Nano board appears powered up via the VIN supply, and similarly everything  is powered by the VUSB supply if that's all that is available. If both are available, then everything is powered by the VIN supply since there's not a diode drop of voltage difference between VIN and VUSB.

    Have I misunderstood the requirement? Or the circuit?

    EDIT: Having re-read, I think you're saying you wish to connect 5V, not a higher VIN (which has to be probably ~ 6V or higher for a regulated output). In that case, you could wire your 5V supply directly to the +5V connection, if you don't use the VIN pin at all. The IC2 (LM1117) might be ok with this (I've not checked the LM1117 datasheet). Worst case, it could be desoldered off, but I suspect it should be fine. Worth a try!

     

    7266.contentimage_207301.png

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 5 years ago in reply to shabaz

    I missed that on the Nano schematic - I looked at the PDF on the official site and the auto-selector circuit is tucked up at the top partially obscured by something else!  But, yes that would give the protection if I used a Nano, great find thanks. 

     

    On the Mega, there doesn't appear to be such a circuit.  There's a diode between the DC connector and VIN; and the USB and VIN is selected through a comparator and FET (basically, if VIN is > 2x3.3V then it wins.)  The best it gives is a poly fuse (F1) and I don't think I could rely on that body diode in the FET.

    3343.contentimage_207302.png5428.contentimage_207303.png3857.contentimage_207304.png

     

    So you're right, I want to use the 5V pin with a regulated 5V supply, and I don't want to use Vin (or a DC connector); I don't even want to power from USB, just be able to communicate to the board whilst it's powered on in-circuit.  The Nano works fine because of that diode.

     

    My choice will come down to memory - the Nano Every has 48KB + 6KB which may be enough; if it isn't I would have to shift up to the Mega.  Using Vin would bring power dissipation concerns (and expense!) into play so whilst I could do it, it would be a bit of a pain.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 5 years ago

    To wrap this up, I think the easiest thing to do is provide footprints for a USB-UART circuit so that if necessary I can bypass the USB power issue altogether!  Something like a Microchip MCP2221a.

     

    I can't work out whether that should be powered from the USB VBUS or whether I can power it from my own 5V supply (preference); nor whether the ground connections for the USB connector, MCP2221a and the Arduino (or MCU) should be the same even if powered from different sources (I always get confused by that!).  I'd rather just connect the D+, D- and GND and leave the VBUS disconnected as not needed.

     

    EDIT: Providing this, where +5Vdd and -Vdd is used as power connections for everything (MCP2221A, Arduino/MCU, USB connector), ignoring USB power, looks like a good fallback position that might cost a couple of quid to add to a PCB if needed.

     

    5504.contentimage_207305.png

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to Andrew J

    Hi Andrew,

     

    If you're planning to use a USB-UART chip like this, an option could be to use the USB supply for only powering up the MCP2221A chip. It seems the easiest, since there will always be power available via USB if is connected, and the MCP2221A chip is doing nothing when the USB connector is not plugged in anyway.

    In other words, you could power the MCP2221A via USB, and power the remainder by whatever is required/preferred for your project (USB or other supply or both), and the USB connector GND and MCP2221A VSS and the remainder circuit ground will still be connected all together, since that's the reference for the RX/TX signals. I wasn't sure if -Vdd is ground or a different voltage in the diagram.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 5 years ago in reply to shabaz

    Hi Shabaz,

     

    That makes a lot of sense given the way I've drawn it, but I've spent some more time thinking through the right approach.

     

    I'm not sure yet whether a 5V MCU will turn out to be the right solution - memory issues, pin counts etc - so I've provided an option for VDD being 3.3V.  That gives me access to a greater range of MCUs, LCDs with built in processors, and so on.

     

    I have a jumper to link VDD and VUSB on the MCP2221A if VDD is 3.3V.  If I power VDD with VBUS and VUSB with 3.3 I think there will be an issue as the internal 3.3 LDO won't be disabled; also Rx and Tx will be 5V levelled and I would want them to be 3.3V levelled.  In a tradeoff, having the chip powered but doing nothing is not ideal but I'd rather that than have problems if I have to power it with the lower voltage.  Hope I've explained that well enough.

     

    -VDD is ground tied to the +5V (or +3.3.V) regulator.

     

    Here's a more complete schematic of this section.  VDD will be either +5V or +3.3V; JP1 will be populated 1 to 2 if it's +3.3V and 2 to 3 if 5V.  I suppose I could also jumper VDD pin between +Vdd and VBUS so that if 5V is used, then I could run the IC off VBUS. 

    2772.contentimage_207306.png

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to Andrew J

    Hi Andrew,

     

    I see what you mean, it makes sense for the two scenarios (3.3V and 5V logic).

    I tried creating a standalone USB-UART, for both logic levels, and I used a separate voltage regulator as shown in the circuit diagram below.. but I've also been dropping this circuit into microcontroller projects as-is, but hard-wired to the correct logic levels without the jumpers shown in the circuit below. It doesn't add much to the cost since it's a very cheap LDO, but admittedly it is a bit unnecessary if the 3.3V supply is available elsewhere!

     

    Recently I've decided to try to use a different USB-UART chip (Cypress Cy7C65213) since it supports a few features I wanted for a specific project (in particular flow control pins) I have not tested it yet. For that too I've just gone with adding the 3.3V LDO.. the unnecessary "luxury" option but I don't lose much sleep over it since I'm not doing anything price-sensitive, and has the slight benefit that it's decoupled from the microcontroller supply.. sometimes that might run at 3V or something I suppose, if it's running off a battery etc. It could be an option if you can't entirely predict how you may use the project or the board may be used for other purposes one day. Using the existing supply on the board makes total sense too.

    3463.contentimage_207307.png