Arduino
  • Products
  • More
Arduino
Arduino Forum Favorite Arduino shields?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 419 subscribers
  • Views 877 views
  • Users 0 members are here
  • hackerspace
  • maker
  • avr
  • make
  • diy
  • shield
  • jimmieprodgers
  • arduino
  • atmel
  • lolshield
Related

Favorite Arduino shields?

fustini
fustini over 16 years ago

Fantastic to have an Arduino group on element14 now.  I hope it will bring more of the DIY maker & hackerspace community into the fold.

 

I've been playing around with PIC & AVRs for couple years now.  Recently, I picked a LoL Shield (130 charlieplexed LED display) from the great Jimmie Rodgers and decided it was time to finally jump into the world of Arduino.

 

Here's previous post I wrote on the LoL Shield:

 

http://www.element-14.com/community/groups/open-source-hardware/blog/2010/05/28/open-source-hardware-kit-lol-shield

 

What are other shields that people have used and would recommend?

 

Thanks,

Drew

http://twitter.com/pdp7

  • Sign in to reply
  • Cancel
  • cookieglitch
    cookieglitch over 16 years ago

    I haven't used one yet, but from what I've been told the ethernet shield is good. Not so sure about native DHCP support, but as usual there are plenty of other libraries around that support it.

     

    As for the LoL shield, it does look good, I think I'm going to have to stick with a bunch of 595s on another board for a current project though sadly

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • nimbusgb
    nimbusgb over 15 years ago in reply to cookieglitch

    I have a couple of BlackWidow Arduinos with integrated Wifi.

     

    Excellent for home energy monitoring and other remote projects.

     

    Output under construction here http://www.imolesworth.info/environment/sample.html ( it may come and go as I tinker with the hardware image )

     

    I'm also using the Arduino in 3 differnet applications aboard a yacht to monitor and control stuff wirelessly

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 15 years ago in reply to nimbusgb

    Very interesting.  I like this BlackWidow board - I hadn't seen it before.  Slick how you have use it to feed data logging & graphing.  Reminds me of the Tweet-A-Watt mod by Lady Ada.

     

    But I gotta saw the marine applications sound even more interesting... do you call it an Yachtuino? image

     

     

    Cheers,

    Drew

    http://twitter.com/pdp7

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tronixstuff
    tronixstuff over 15 years ago

    I like the Freetronics Ethernet shield from Australia, which supports PoE as well. www.freetronics.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago

    This is simple but handy prototyping shield that I've used in the past for the mega: http://www.nkcelectronics.com/arduino-megashield-pcb.html