Arduino Forum Arduino is not a frend to ESP8266
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
  • Replies 10 replies
  • Subscribers 403 subscribers
  • Views 1209 views
  • Users 0 members are here
Related

Arduino is not a frend to ESP8266

Former Member
Former Member over 9 years ago

For four days trying to communicate esp 01, unsuccessfully, I already changed and firmeware. I use Arduino and I never have any problems with sensors to Arduino or ESP is complicated. the only thing I managed to get through communication Arduino IDE serial AT komands

I do not know if I have a problem with Hardwear or softweare

Interests proven example of programming of ESP 01 which firmevarom and how to set up the Arduino IDE.

Connected to the scheme, with a separate power supply 3.3V

Who can help me here thanks in advance.

 

 

Or I'll leave and throw it in the trash

 

Tnx Damir

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 9 years ago +2
    You have not much information here, so check shinajaran: noob's guide to ESP8266 with Arduino Mega 2560 or Uno . It explains things step by step. Clem
  • clem57
    clem57 over 9 years ago in reply to Former Member +2
    Think Tx is talking and Rx is ear to listen. When I talk(Tx), you listen with ear(Rx). Right? Clem
  • Former Member
    Former Member over 9 years ago +2
    I got it. Connected to the scheme on the serial port ardu going gets feedback from ESP AT commands. But when I want to program esp occurs fault serial is not in sync. chart below.
Parents
  • Former Member
    Former Member over 9 years ago

    I got it. Connected to the scheme on the serial port ardu going gets feedback from ESP AT commands. But when I want to program esp occurs fault serial is not in sync.

    chart below.

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 9 years ago

    I got it. Connected to the scheme on the serial port ardu going gets feedback from ESP AT commands. But when I want to program esp occurs fault serial is not in sync.

    chart below.

     

    image

    • Cancel
    • Vote Up +2 Vote Down