Arduino
  • Products
  • More
Arduino
Arduino Forum Have a question about Arduino? Ask me!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1914 replies
  • Subscribers 528 subscribers
  • Views 68519 views
  • Users 0 members are here
  • jeremy_blum
  • expert
  • student
  • arduino
Related

Have a question about Arduino? Ask me!

sciguy14
sciguy14 over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Questionabout Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

Jeremy Blum

Jeremy is an Electrical and Computer Engineering Student at Cornell University. He has been building microcontroller projects since high school, from a prototype prosthetic hand with a novel control scheme, to a nerf gun that fires at the intruders and uploads their picture to the web.
  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +2
    @Brendan Your video is somewhat adequate for the intended purpose, however, from an engineer's point of view it is lacking in providing pertinent facts. Such as the part number, data sheet, and source…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Jeremy, thanks for your intro videos. I am just getting started myself in Arduino though I have done some simple electronics projects using Atmel chips. Here is an example using ATTiny13 chips. www.youtube…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi Jeremy I've built a device (see picture) with an Arduino and Ethernet shield that connects to our Network Monitor (Nagios) and moves an arrow to indicate if any of the computers we monitor are not responding…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi Jeremy,

    Firstly let me thank you for all your tutorial videos on Arduino. I have watched most of them and find them very helpful.

     

    I have been asking for advice in the Arduino forums but not getting anywhere, you’re my last hope!

     

    Arduino is quite new to me, I’ve only been playing for 6 months or so. I have taken on a large project based on a standard 8x8 matrix, I’ve simply upgraded it to a large 8x8 display, all homemade.

    I love the hardware side of these projects, soldering and sorting out power feeds is great fun. The code however is a very different animal.

     

    I'm stuck on the last bit of my project which is a Christmas present for my mum, so needs to be completed in the next day or two. I need some advice urgently if you could spare the time?

     

    Because I can’t code myself, I’ve had to cut and paste code from other people’s projects and this is where the problem lies.

     

    I have code which works correctly to play pong on my 8x8 matrix. I also have code to simply display an effect. What I'm trying to do is to have a button so that when it's pressed it will switch between the two modes. The best I’ve achieved so far is to have is to have it begin with pong, when the buttons pressed it switches to pattern, then the button gets ignored.

     

    NB, Not so important but it would also be nice to be able to choose the size of the paddles (set to 2 at least) and have the pattern displayed by default until the button is pressed.

     

    Please could you take a look at this code and try to work out what’s going wrong? My back is really against the wall, if you can/want to help, please do so quickly.

     

    All the best,

    Phillip

     

     

    Code is in the attached txt file.

    Attachments:
    jereny-help.txt.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fischerjade
    fischerjade over 13 years ago in reply to e14 Contributor

    I just got a arduino UNO and I ran the Blink program from Makezine.  It worked but now I can't load another program from the arduino IDE from my mac.  The board just keeps blinking the light on the board.  When I push the reset button it just stops the program briefly and starts over again. I need to reset the chip/board somehow or am I doing it wrong I am a newbie.

     

    Jade Fischer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fischerjade
    fischerjade over 13 years ago in reply to e14 Contributor

    I just got a arduino UNO and I ran the Blink program from Makezine.  It worked but now I can't load another program from the arduino IDE from my mac.  The board just keeps blinking the light on the board.  When I push the reset button it just stops the program briefly and starts over again. I need to reset the chip/board somehow or am I doing it wrong I am a newbie.

     

    Jade Fischer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to fischerjade

    I'm also a newbie but I guess you have to just upload the other program and ... that's all !