Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Have a question about Arduino? Ask me!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1914 replies
  • Subscribers 527 subscribers
  • Views 69694 views
  • Users 0 members are here
  • jeremy_blum
  • expert
  • student
  • arduino
Related

Have a question about Arduino? Ask me!

sciguy14
sciguy14 over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Questionabout Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

Jeremy Blum

Jeremy is an Electrical and Computer Engineering Student at Cornell University. He has been building microcontroller projects since high school, from a prototype prosthetic hand with a novel control scheme, to a nerf gun that fires at the intruders and uploads their picture to the web.
  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +2
    @Brendan Your video is somewhat adequate for the intended purpose, however, from an engineer's point of view it is lacking in providing pertinent facts. Such as the part number, data sheet, and source…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Jeremy, thanks for your intro videos. I am just getting started myself in Arduino though I have done some simple electronics projects using Atmel chips. Here is an example using ATTiny13 chips. www.youtube…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi Jeremy I've built a device (see picture) with an Arduino and Ethernet shield that connects to our Network Monitor (Nagios) and moves an arrow to indicate if any of the computers we monitor are not responding…
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Ok, I've got a question about the capibilities of Arduino.  I'm in the planning stage to build a USB racing steering wheel controller.  It requires precision and reactive inputs & outputs to a control feedback system.  My concern about Arduino being used as the controller came in after watching how servo motors react to the output from the Arduino after the input data from a POT is taken.  There seems to be a very small delay be the change in data from the POT and the response by the servo motor.  If I use Arduino as a controller can I expect this type of delay or is this an issue with the servo motor response?

     

    Reference Video:

    http://www.youtube.com/watch?v=FKj9jJgj8Pc

     

    Thanks for any response or direction

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • sciguy14
    sciguy14 over 15 years ago in reply to e14 Contributor

    If you really really need fast response times, you should look into programming an atmega in C directly using an ICSP (In circuit serial programmer).  An atmel programmed in C can swith outputs much faster than an arduino due to the nature of the simplified arduino language.  Alternatively, you can try implementing C code directly on an arduino using this tutorial: http://arduino.cc/en/Hacking/Programmer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • terryking
    terryking over 15 years ago in reply to sciguy14

    @Neokinetic: The example you saw on YouTube has a 15 millisecond delay every loop. Even so it seems pretty fast. I'l quite sure you are mainly seeing the Servo response time. Servo specs will tell you the time for a specific motion.

     

    Without the delay Arduino will be checking that pot 1000+ times per second.  I would put the hardware together and work on optimizing the Arduino code before going towards Assembler or direct 'C'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • terryking
    terryking over 15 years ago in reply to sciguy14

    @Neokinetic: The example you saw on YouTube has a 15 millisecond delay every loop. Even so it seems pretty fast. I'l quite sure you are mainly seeing the Servo response time. Servo specs will tell you the time for a specific motion.

     

    Without the delay Arduino will be checking that pot 1000+ times per second.  I would put the hardware together and work on optimizing the Arduino code before going towards Assembler or direct 'C'.