Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Have a question about Arduino? Ask me!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1914 replies
  • Subscribers 527 subscribers
  • Views 69965 views
  • Users 0 members are here
  • jeremy_blum
  • expert
  • student
  • arduino
Related

Have a question about Arduino? Ask me!

sciguy14
sciguy14 over 15 years ago

This thread has been closed to new questions.

However, we welcome you to Post Your Questionabout Arduino in the element14 Community Arduino group.  You'll find many fellow members and experts who have just the answer you're looking to find! 

 

Thank You, Your Friends at element14 Community


image

Jeremy Blum

Jeremy is an Electrical and Computer Engineering Student at Cornell University. He has been building microcontroller projects since high school, from a prototype prosthetic hand with a novel control scheme, to a nerf gun that fires at the intruders and uploads their picture to the web.
  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to e14 Contributor +2
    @Brendan Your video is somewhat adequate for the intended purpose, however, from an engineer's point of view it is lacking in providing pertinent facts. Such as the part number, data sheet, and source…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Jeremy, thanks for your intro videos. I am just getting started myself in Arduino though I have done some simple electronics projects using Atmel chips. Here is an example using ATTiny13 chips. www.youtube…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    Hi Jeremy I've built a device (see picture) with an Arduino and Ethernet shield that connects to our Network Monitor (Nagios) and moves an arrow to indicate if any of the computers we monitor are not responding…
  • bobcroft
    bobcroft over 15 years ago

    Jeremy,  can the AVR studio 5 be used for programming the Arduinos instead of the basic Arduino IDE?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to bobcroft

    Hi,

    what is a problem? now I buy a new chip ATMEGA328P-PUATMEGA328P-PU, my arduino uno works good,but can't upload job, I see problem text:

    Binary sketch size: 1018 bytes (of a 32256 byte maximum)
    avrdude: stk500_getsync(): not in sync: resp=0x00
    avrdude: stk500_disable(): protocol error, expect=0x14, resp=0x51

     

    How fix this problem?

    thanks for answer

    Bye

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dmaruska
    dmaruska over 15 years ago in reply to e14 Contributor

    Where did you buy the chip, was the Boot loader already installed?  If not I would start there.

     

    Regards,

     

    Dave M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bobcroft
    bobcroft over 15 years ago in reply to e14 Contributor

    Hi,  I had exactly the same problem with a FreeDuino board.  check that you have the correct board and COM port selected.  I also slowed down the serial data rate in the 'boards' file from 115200 to 57600.  Try googling the error message there are a number of threads.

     

    It appears this fault (error) is common on the Arduino but I could find no definitve fix. However when I slowed down the serial transmission speed it fixed the Freeduino BUT this used the FTDI chip to translate USB to serial.  I bel;ieve the Arduino uses a different chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi Jeremy  ,

    Firstly many   Thanks  for  your Tutorials.
    Just  worked  through  the  first switch program  example.  Just   reading the  switchPin  on pin 8 and  then lighting up  to the LED  on   pin 13 . Worked  fine .

    Strange  Behaviour
    Just playing about   I  connected  it   to pin 9    without  changing  the program  and  it  worked !   so  I  tested the  other  pins  and   they   did no work (good). WHY?

    Then  just to make  sure   I made   pin 9  output .   This  time it    did  not  light  up .  But  after a  few  clicks   it did . (even  though  it is configured as OUTPUT). WHY?

    Thanks

    Tariq

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi,

    how sent bootloader in my new ATMEGA328P-PUATMEGA328P-PU, I don't have a parallel programmer, i have just arduino uno, can I use it board?

    thanks in advance

    BR/Ugnius

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    hi, i inted to create a nano second delay using arduino how can i do it. because it has functions such as delay()-which produces delay in milli seconds.. delayMicroseconds()-which produces delay in micro seconds if we want to produce in nano seconds what can we do? the delayMicroseconds() function is sensitive only in parameters which are multiples of four... if i need to get a delay for each microseconds what can i do? please help me...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    The clock speed of an arduino is 16 MHz. That's a clock period of 62.5 ns. You can't do nanosecond delays with code.

     

    Sent from my iPad

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    How would one connect something like this SRF02 to an Arduino?

    http://www.acroname.com/robotics/parts/R287-SRF02.html

    Is there some kind of connector that would make soldering unnecessary?

    Thanks for all your help. Those video tutorials are great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    what all are components required to build a robot along with arduino board for the beginners??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>