Arduino
  • Products
  • More
Arduino
Arduino Forum Did I get this right?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 420 subscribers
  • Views 800 views
  • Users 0 members are here
Related

Did I get this right?

e14 Contributor
e14 Contributor over 15 years ago

Ok the object is to display the temp in C & F on a 3 digit 7 segment display using the following.

 

Arduino Uno

Ds18b20 - digital One wire temp sensor

(2) 74HC_HCT595 - shift register

1k resistor network (shown under the LED)

3 digit 7 segment common cathode LED display

SPST NO MC switch

A few other odds & ends (see pic)

 

Total noob here so all input or better ways to do this is welcome!

 

image

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • simon.monk
    simon.monk over 15 years ago

    Hi Meden,

     

    Unless you are using your other Arduino pins for something else, you definately don't need the shift register to drive the transistors. A 270R resistor from base to three output pins on the Arduin will work just fine.

     

    You don't need the other shift register either, unless your LEDs are high current, you can just use eight outputs from the Arduino through the series resistors, as long as you are not taking more than 40mA per segment.

     

    For example software for driving 4 digits in this way, download the sketches from http://www.arduinoevilgenius.com and look at project 30.

     

    http://2044900894781404227-a-1802744773732722657-s-sites.googlegroups.com/site/arduinobook/projects/F09-15.jpg?attachauth=ANoY7cqgpB4LhtieRZbTmNYCn4O47I_75QJ-ux8fVGH_L_WtFbKtjJu2LeYD_h3yDoNCEk72-3b8Kb0BGg0_bwYHpJ6WB7FzduTEq80lTvuQ5GtqQUHK9TDawIEn3dOqGlPqIy9lpnHvOiFC9_jjrT1zA5rVBt8dJN7MkLv4hnxt9pN7_5cNuTwvWTjLikx7Fd8cpYLU-MlXmncMGFdMHJveR24ZyLLTPw%3D%3D&attredirects=0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to simon.monk

    The completed project will be a climate control for a car. Consisting of 10 buttons to control acuators and a servo. The  system will read inside and outside temp. and adjust acordingly. I was  thinking of using another shift register for the buttons. I'd like to  keep the pin usage as minimal as possible and code lean and tight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to simon.monk

    The completed project will be a climate control for a car. Consisting of 10 buttons to control acuators and a servo. The  system will read inside and outside temp. and adjust acordingly. I was  thinking of using another shift register for the buttons. I'd like to  keep the pin usage as minimal as possible and code lean and tight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • simon.monk
    simon.monk over 15 years ago in reply to e14 Contributor

    Hi,

     

    10 butons - 7 pins (buttons in 4 x 3 array - there is an Arduino library for key matrix)

    Actuator and servo - 2 pins

    LED segments - 8 pins

    LED common transistors - 3 pins

     

    Makes 20 pins image

     

    Only 18 available on the Arduino - you can use the Analog Ins as outputs too.

     

    So maybe keep the shift register for the segments.

     

    The more hardware, the more chance of something failing. Once the software is right, it stays right!