Arduino
  • Products
  • More
Arduino
Arduino Forum Did I get this right?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 420 subscribers
  • Views 793 views
  • Users 0 members are here
Related

Did I get this right?

e14 Contributor
e14 Contributor over 15 years ago

Ok the object is to display the temp in C & F on a 3 digit 7 segment display using the following.

 

Arduino Uno

Ds18b20 - digital One wire temp sensor

(2) 74HC_HCT595 - shift register

1k resistor network (shown under the LED)

3 digit 7 segment common cathode LED display

SPST NO MC switch

A few other odds & ends (see pic)

 

Total noob here so all input or better ways to do this is welcome!

 

image

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • jnissen
    jnissen over 15 years ago

    Or go with a LCD in 4 bit mode to save some pins. Lower current as well and you can get nice backlit versions. Then of course you have actual text messages instead of numbers to make it more friendly. The LCD is really easy to use with the library. My son managed to talk to the LCD in only a few nights and he had never done any controller work in the past. Give it a try.

     

    Another possible thing is to multiplex the 8 lines for the LED segments with button scanning. You can scan the buttons so quickly the eyes will never detect you actually turned off the LED's and were using the bits to scan buttons! I've done this type of thing in the past but it adds complexity as you need to add a 8 input/16 output/1 control line mux to the wiring. Use two of these: http://www.rohm.com/products/databook/general/pdf/bu4551b-e.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jnissen
    jnissen over 15 years ago

    Or go with a LCD in 4 bit mode to save some pins. Lower current as well and you can get nice backlit versions. Then of course you have actual text messages instead of numbers to make it more friendly. The LCD is really easy to use with the library. My son managed to talk to the LCD in only a few nights and he had never done any controller work in the past. Give it a try.

     

    Another possible thing is to multiplex the 8 lines for the LED segments with button scanning. You can scan the buttons so quickly the eyes will never detect you actually turned off the LED's and were using the bits to scan buttons! I've done this type of thing in the past but it adds complexity as you need to add a 8 input/16 output/1 control line mux to the wiring. Use two of these: http://www.rohm.com/products/databook/general/pdf/bu4551b-e.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • cookieglitch
    cookieglitch over 15 years ago in reply to jnissen

    For the LCD, there is also the option of using something like Sparkfun's LCD backpack (http://www.sparkfun.com/products/258). Reduces the number of pins down to one by sending all the data over the TX line. It is essentially just a pic with their software on so not too hard to do yourself if you feel inclinded to do so. Where the number of pins is an issue, it is certainly useful!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to cookieglitch

    The car this is going in is a Lamborghini Countach 25th Anniversary which had an LED display that I'm attempting to replicate. The second version will use a LCD display and be used in a Diablo Replica. I'm looking into possibly using the analog pins as digital pins using this ...

     

    http://arduino.cc/en/Tutorial/AnalogInputPins

     

    Thanks for your help simon, jnissen, and John