Arduino Forum Arduino 32bits cards available from Digilent
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
  • Replies 6 replies
  • Subscribers 404 subscribers
  • Views 534 views
  • Users 0 members are here
  • open-source
  • microchip
  • ethernet
  • usb
  • prototyping
  • shield
  • pic32
  • arduino
  • pic
  • opensource
Related

Arduino 32bits cards available from Digilent

MicrochipRTCfr
MicrochipRTCfr over 14 years ago

Hi,

 

Looking for a 32bits / 80MHz Arduino with plenty of FLASH & RAM  ( 512K / 128K ), Ethernet, USB, CAN ... ?

 

You can immediately get it from Digilent ;=)

 

regards

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 14 years ago

    But the board is not 100% compatible....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bobcroft
    bobcroft over 14 years ago in reply to Former Member

    frankman,

                   could you elaborate please.  Exactly what is not 100% compatible?  It is also my impression that not all of the Arduino clones are 100% compatible either.  I am interested because as a newbee to the Arduino I prefer not to buy something that may give me problems if I did not use the original UNO.  This diligent board looks to be a good price point for a complete board i.e. not a kit.

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 14 years ago in reply to bobcroft

    Hi,

     

    The ChipKit Uno32 and Max32 have some pins with 3.3V max which is why they may have some compatibility issue with some boards.

     

    Digilent has just released a ChipKit Basic I/O shield to take advantage of the many peripherals on board on the PIC32.

     

    Another one is under development and will offer CAN, Ethernet and USB ;=)

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • MicrochipRTCfr
    MicrochipRTCfr over 14 years ago in reply to MicrochipRTCfr

    Hi

     

    The Chipkit Network shield is also available now. It enables Ethernet, USB and CAN when combined with the Chipkit MAX32

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • MicrochipRTCfr
    MicrochipRTCfr over 14 years ago in reply to MicrochipRTCfr

    Hi

     

    The Chipkit Network shield is also available now. It enables Ethernet, USB and CAN when combined with the Chipkit MAX32

     

    Regards