Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino 32bits cards available from Digilent
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 419 subscribers
  • Views 769 views
  • Users 0 members are here
  • open-source
  • microchip
  • ethernet
  • usb
  • prototyping
  • shield
  • pic32
  • arduino
  • pic
  • opensource
Related

Arduino 32bits cards available from Digilent

MicrochipRTCfr
MicrochipRTCfr over 15 years ago

Hi,

 

Looking for a 32bits / 80MHz Arduino with plenty of FLASH & RAM  ( 512K / 128K ), Ethernet, USB, CAN ... ?

 

You can immediately get it from Digilent ;=)

 

regards

  • Sign in to reply
  • Cancel
Parents
  • chgus
    chgus over 14 years ago

    Got my chipkit UNO32 today. image Worked well and blinked the led as it was powered up. I was very surprised when i was not able to program my UNO32, MPIDE reported: image

     

    avrdude: verification error, first mismatch at byte 0x0180

             0x00 != 0xff

    avrdude: verification error; content mismatch

     

     

    avrdude: verification error, first mismatch at byte 0x0180
             0x00 != 0xff
    avrdude: verification error; content mismatch

    Due to some firmware/chip timing problem that has been known for quite a long time now, the programming failed. Not shure how long my unit has been sitting on the shelf, but i thougt this should have been caught at factory QA. Not a biggie if it could easily be upgraded with the new (downloadable) firmware, but it turn out that i need an ICSP programmer - which i don't have. A second inconveience is that the UNO32 is missing the ICSP connector, the connector itself is not soldered onto the board. The chipkit wiki had a page describing the problem, couldn't find anything about it on the diligent website.

    My UNO32 unit has a barcode label "D387905" that i suppose is the serial number.

     

    Are Diligent still shipping units with outdated firmware?

    Is this a common problem?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 14 years ago in reply to chgus

    Hi Cris,

     

    I have used my UNO32 for several months and have not had any problems using the USB interface with the software provided by the Diligent web site.  I have not used the MPIDE, but mine worked fine just from the IDE.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB over 14 years ago in reply to chgus

    Hi Cris,

     

    I have used my UNO32 for several months and have not had any problems using the USB interface with the software provided by the Diligent web site.  I have not used the MPIDE, but mine worked fine just from the IDE.

     

    DAB