Arduino
  • Products
  • More
Arduino
Arduino Forum Emergency!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 417 subscribers
  • Views 618 views
  • Users 0 members are here
  • board
  • coding
  • of
  • gravity
  • the
  • to
  • sensors
  • timer
  • ldr
  • led
  • calculate
  • arduino
  • laser
  • earth
  • two
  • using
  • advice
  • photoresistor
Related

Emergency!

dirtdiver
dirtdiver over 15 years ago

Hello everyone, I'v been given a school project:

  

       calculate the gravity of earth using two sensors to estimate the time needed for a free falling object to go from sensor1 to sensor 2.

Now, I'm gonna use 2 photoresistors and 2 lasers ,can anyone suggest how to measure that time?

Can that value be displayed on a pin when I debbug it?

 

I need to make that project fast so any advice is appreciated!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Hi,

     

    I am new here so sorry if I talk slightly off the topic. I work with PIC never with Arduino but if I was given assigment like this I would do it using system timer. Depending on what degree of accuracy is expected set the prescaler to proper value and if object crosses first set of, lets call it barrier, it will reset timer to 0 (zero), then if object cross second set copy the value of timer to variable. After this you have to multiply value from variable times impulse timing. This will give you total object falling time across distance between two barriers. Hope that makes any sense image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 15 years ago

    Before you get too carried away with the hardware -  work out how you are going to calculate g from the transit time between two points - I'll tell you now for free that it can't be done without making some assumptions that may be hard to keep to in practice and will dictate exactly how you set up the experiment.

    If your school has a modern oscilloscope you don't actually need to build anything.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 15 years ago in reply to michaelkellett

    Well , I only need to find out what the time is. The calculations are in someone elses hands

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago

    Photoresistors have relatively slow response and lasers are very much overkill. An LED or flashlight along with a photodiode or perhaps a CdS cell (if it is fast enough) will be fine.

     

    The Arduino has a function that will give you the current time in miliseconds or microseconds. Look at: http://www.arduino.cc/en/Reference/HomePage

     

    pseudo code:

    1. Wait for sensor 1 to detect falling object.

    2. record time t1=millis(); Or you can use micros().

    3. Wait for sensor 2 to detect falling object.

    4. record time t2=millis();

     

    5. dt=t2-t1.

     

    You can't display anything on a pin; you can control the signals going to a pin. Just use the Serial port to send the dt value back to the console.

     

    6. Serial.println(dt).

     

    This will give you the average velocity between the two sensors. You'll need to know how far the object has fallen before it gets to sensor #1. In addition, the farther you make the separation between sensor #1 and #2, the better your accuracy will be.

     

    A better experiment is to simply build a pendulum and measure it's period with a single sensor. The experiment will be smaller and probably give you a more accurate estimate of g.

     

    Not sure how this is an emergency, by the way.

     

    -Scott