Arduino
  • Products
  • More
Arduino
Arduino Forum Tutorial 5 the NPN Transistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 420 subscribers
  • Views 3750 views
  • Users 0 members are here
  • transistor
  • help
  • npn
  • 2n7052
  • (
  • arduino
Related

Tutorial 5 the NPN Transistors

dirtdiver
dirtdiver over 14 years ago

I cant seem to find a 2N70522N7052 npn transistor (the one used it the video for the dc motor)

  • BIPOLAR TRANSISTOR, NPN, 100V
  • Transistor Polarity: NPN
  • Collector Emitter Voltage V(br)ceo: 100V
  • Transition Frequency Typ ft: 200MHz
  • Power Dissipation Pd: 625mW
  • DC Collector Current: 1.5A
  • DC Current Gain hFE: 10000
  • RoHS Compliant: Yes

 

Can I use a  different one?

  • Sign in to reply
  • Cancel

Top Replies

  • MDeGrauw
    MDeGrauw over 14 years ago +1
    Check at bf.farnell.com I guess they will have it in catalog.
  • MDeGrauw
    MDeGrauw over 14 years ago in reply to MDeGrauw +1
    Sorry bg.farnell.com
  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver +1
    Yes, it will work with different transistor with similar specifications as original. This transistor will act as the low voltage and low current to high voltage and high current bridge. Just insure the…
Parents
  • MDeGrauw
    MDeGrauw over 14 years ago

    Check at bf.farnell.com

    I guess they will have it in catalog.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • MDeGrauw
    MDeGrauw over 14 years ago in reply to MDeGrauw

    Sorry bg.farnell.com

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to MDeGrauw

    I found it BUT its going to cost me 20$ to deliver it, the transisitr is 0.7$ image

    will it work if I get different transistor with the same characteristics (and if yes wich of them are important in my case)

    thanks in advance!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver

    Yes, it will work with different transistor with similar specifications as original.  This transistor will act as the low voltage and low current to high voltage and high current bridge.  Just insure the current of the transistor is NOT less than the motor you’re going to drive.  If you are going to PWM the motor, insure the transistor will operate correctly with the frequency you will be at.

     

    Dave M.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to dmaruska

    so I'm gonna be using a dc motor (just like in the tutorial-with the diod and the capasitor)  That motor is consuming 70 mA  so I need a transistor that can supply atleast that much current right? And what is the frequency I need (it will be controlled with the Arduino with PWM-again, just like in the tut.)

    Thanks alot!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver

    All of the Trasistors will work for the PWB that you will be at.  The one above has a max frequency of 200Mhz.  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to dmaruska

    so the frequency doesnt metter much in my case?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver

    No, you will be ok.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to dmaruska

    Ok man thanks alot just one more thing , can I connect not 1 but two motors (parallel) of course I will need a transistor that can support the currnet consumption, but I wont need x2 of the capasitors and the diods

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver

    The cap and diode is for noise and transistor protection.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to dmaruska

    so this should be fine then right?image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to dmaruska

    ok I think I found some suitable substitutes   -  2N67152N6715 , 2N70522N7052 , BD135GBD135G

     

    what do you think?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dirtdiver
    dirtdiver over 14 years ago in reply to dmaruska

    ok I think I found some suitable substitutes   -  2N67152N6715 , 2N70522N7052 , BD135GBD135G

     

    what do you think?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver

    Yes these will work.  I personally would not place two motors in parallel, I would drive with one transistor each, but you can drive from the same bit (digital) line.  Though it will work, just not proper.  If you noticed the orginial transistor was a darlington pair (two transistors in same package), which gave the gain hfe such a high number.  But these will work just fine.  Monitor Transistor for heat.  If it gets hot, use a head sink.  The BD135GBD135G has a hole that you can screw a piece of aluminum to help if needed. Good luck.

     

    Regards,

     

    Dave M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to dmaruska

    Thanks Dave! That wasreally helpful !!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver

    Hope all works out good for you.  I'm a hardware guy that is just now getting in to the software side of things.  Jeremy's tutorials are very nice.  Have anymore questions, I will help if I can...

     

    Regards,

     

    Dave M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to dmaruska

    Oh, there is something else-  how to reverse the motor  (without having to switch the + and -)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver

    In the tutorial, Jeremy speaks of and "H" block.  This is what is used to add forward and reverse to a motor control.  If you get real crafty and want to do it yourself, you can build a circuit, but "H" block is the proper way to do this.  It has 4 Transistors (usually MOSFET's)  and a few other parts for this.

     

    Regards,

     

    Dave M.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to dmaruska

    Its actually called an "H - Switch" or "H - Bridge, even if it is portrayed in a "block!"

    A simple one can be viewed here:-

    http://www.instructables.com/id/How-to-make-an-H-bridge/

    A good explanation can nbe found here:-

    http://en.wikipedia.org/wiki/H_bridge

    I hope this helps.

    regards

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to e14 Contributor

    thanks for the replay ! very useful!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to dmaruska

    i found a suitable transistor but how to determite witch pin is the emitter and witch is the collector

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    The data sheet should tell you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dmaruska
    dmaruska over 14 years ago in reply to dirtdiver

    Agree with R_Phoenix.  Get the Data sheet, and keep it for all components that you work with.