Arduino
  • Products
  • More
Arduino
Arduino Forum I killed a mouse
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 418 subscribers
  • Views 977 views
  • Users 0 members are here
Related

I killed a mouse

chgus
chgus over 14 years ago

Hi,

 

I recently gave some advice in another thread on reading the wheel from a wheel mouse (i think). Since I have seen no confirmation that my advice actually worked I went ahead and killed a wheel mouse, found and extracted the wheel encoder. This is how and what I did to read the wheel encoder from the mouse.

 

The wheel encoder from the dead mouse.

image

I made a small breadboard setup just to connect the wheel encoder and the arduino. I have no documentation of any kind on this part. After a short study of how it was connected on the original mouse PCB I had a theory. I named the connectors from left to right "B" "A" and "GND". The orientation of the wheel encoder in my hand matches the three round connections on the drawing below. In my test i used capacitors 1uF, but they seem to be a bit large. The reason for the capacitors is debouncing.

 

image

The waveform that i see when slowly turning the wheel looks like this:

 

image

So, if you trigger an interrupt on changes on the upper signal "A" while also reading "B" in the interrupt routine, You can determine both motion and what direction.

 

How do I determine direction? Turning the wheel is like moving the vertical bar left or right over the waveforms. Every time the upper wave "A" changes level, i also look at "B"  and compare them. If I move right (turn wheel clockwise) I see "B" at the same logic level as "A". If i move left (turn wheel counterclockwise) I will always find "B" at opposite logic level from "A" when "A" changes. Hence the code for this:

 

  a=digitalRead(2);

  b=digitalRead(3);

  if(a==b){

    wheel++;

  } else {

    wheel--;

  }

 

 

My code deliver this output, new line every second. The wheel was turned slowly clockvise.

 

 

Wheel position: 0

Wheel position: 0

Wheel position: 2

Wheel position: 5

Wheel position: 3

Wheel position: 7

Wheel position: 11

Wheel position: 14

Wheel position: 16

Wheel position: 18

Wheel position: 16

Wheel position: 16

Wheel position: 16

 

 

This is the code in my Arduino UNO:
// wheel has 3 connectors
// one connects to ground
// the two others connect to digital pin 2,3

// variable to hold wheel position
volatile int wheel=0;

void setup() {
  pinMode(2,INPUT);
  // internal pull up
  digitalWrite(2,HIGH);
  pinMode(3,INPUT);
  // internal pull up
  digitalWrite(3,HIGH);
  attachInterrupt(0,moved,CHANGE);
  Serial.begin(9600);
}

void loop(){
  int a,b;
  Serial.print("Wheel position: ");
  Serial.println(wheel,DEC);
  delay(1000);
}

// interrupt handler
void moved(){
  int a,b;
  a=digitalRead(2);
  b=digitalRead(3);
  if(a==b){
    wheel++;
  } else {
    wheel--;
  }
}

Enjoy!

 

 

Wheel position: 0
Wheel position: 0
Wheel position: 2
Wheel position: 5
Wheel position: 3
Wheel position: 7
Wheel position: 11
Wheel position: 14
Wheel position: 16
Wheel position: 18
Wheel position: 16
Wheel position: 16
Wheel position: 16
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hey Christer, thanks for sharing this information. I was looking for something like this for a time now and its here. Will try it for sure. Thanks mate!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago

    Hey Christer, thanks for sharing this information. I was looking for something like this for a time now and its here. Will try it for sure. Thanks mate!