Arduino
  • Products
  • More
Arduino
Arduino Forum Upload a parameter to a web page
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 418 subscribers
  • Views 808 views
  • Users 0 members are here
Related

Upload a parameter to a web page

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

My project is to use the Arduino as a datalogger (for temperature and gas consumption).

The temperature measurement and gas counter work fine.

I would like now to transmit these data to a web page.

 

The web page is ready to receive the data : this is the url used with my web brower to transmit data :

http://www.xx/NS1.php?P1=counter_value

When the parameter is received, the web page sends an email.

 

Now I would like to do the same thing with the arduino.

But it doesn’t work : there is no error message but the web page is simply not activated. This is the code used :

 

#include <SPI.h>

#include <Ethernet.h>

 

byte mac[] = {  0xDE, 0xAD, 0xBE, 0xEF, 0xFE, 0xED };

IPAddress server(xx,xx,xx,xx); //my web site IP adress

EthernetClient client;

 

void setup() {

  delay(3000);

  Serial.begin(9600);

  Serial.println("Starting...");

  if (Ethernet.begin(mac) == 0) {

     Serial.println("Failed to configure Ethernet using DHCP");

  }

 

  delay(1000);

  Serial.println("connecting...");

 

  if (client.connect(server, 80)) {

      Serial.println("connected");

      client.println("http://www.xxx.NS1.php?P1=counter_value");

      client.println();

      Serial.println("Request sent");

  }

  else {

      Serial.println("connection failed");

  }

}

 

void loop()

{

}

 

Do you have an idea of what is wrong ?

Thanks for your help.

  • Sign in to reply
  • Cancel
  • fustini
    fustini over 14 years ago

    Do you see the serial output from the Arduino ok?  For example, does it print "connected".

     

    On the server, does the access log for the web server show requests for "http://www.xxx.NS1.php?P1=counter_value"?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to fustini

    You may also want to use this function to print the local IP address after Ethernet.begin():

     

    http://arduino.cc/en/Reference/EthernetLocalIP

      Serial.println(Ethernet.localIP());

    You could then see if you are able to ping the IP address from your computer or, ideally, from the server to see if your Arduino is on the network ok.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Hello thanks for your reply.

     

    Yes on the serial output the messages are displayed : "connected" and "request sent"

     

    I can ping the Arduino from my computer without problem.

     

    Actually I do not have access to server access log.

     

    Thanks again for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    That's too bad about the access log.  It would be good to know if the server receives the request at all or not.

     

    Were you able to run the default Ethernet example?  Were it just does a simple GET from Google?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to fustini

    BTW, you can also call client.connect() with a domain name like client.connect("yourdomain.com", 80) if you want to rule out the off chance that you have the wrong ip address.

     

    Also, when I was troubleshooting the WiFly shield which uses similar library, it was very useful to insert debug serial print statements inside the lower level read and write calls to see all the data that was going back forth.  You might be able to something similar in utility/socket.cpp or utility/w5100.h.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Hello Drew,

     

    The Webclient sample works fine.

    I have just changed IPAddress server(173,194,67,94); // Google

     

    I have tried client.connect("yourdomain.com", 80); // no change

     

    You have right, I must see the server access log.

    I have asked to my provider but no response up to now.

     

    Thanks again for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • benl
    benl over 14 years ago

    What is wrong is that you have to send an HTTP request, not a URL.

     

          client.println("http://www.xxx.NS1.php?P1=counter_value");

          client.println();

     

    should be

     

          client.print("GET /NS1.php?P1=counter_value HTTP/1.0\r\n");

           client.print("Host: xxx.xxx\r\n");

          client.print("\r\n");

     

    (println may do the right thing with the newlines, I don't know).




    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to benl

    Ah ha, it was missing GET.  Nice catch!  I feel bad for not seeing that image   Hopefully this solves dakota77's issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Yes !

     

    It works fine now exactly with the 3 lignes suggested by Ben.

    Thanks a lot for your help