Arduino
  • Products
  • More
Arduino
Arduino Forum Upload a parameter to a web page
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 418 subscribers
  • Views 809 views
  • Users 0 members are here
Related

Upload a parameter to a web page

e14 Contributor
e14 Contributor over 14 years ago

Hello,

 

My project is to use the Arduino as a datalogger (for temperature and gas consumption).

The temperature measurement and gas counter work fine.

I would like now to transmit these data to a web page.

 

The web page is ready to receive the data : this is the url used with my web brower to transmit data :

http://www.xx/NS1.php?P1=counter_value

When the parameter is received, the web page sends an email.

 

Now I would like to do the same thing with the arduino.

But it doesn’t work : there is no error message but the web page is simply not activated. This is the code used :

 

#include <SPI.h>

#include <Ethernet.h>

 

byte mac[] = {  0xDE, 0xAD, 0xBE, 0xEF, 0xFE, 0xED };

IPAddress server(xx,xx,xx,xx); //my web site IP adress

EthernetClient client;

 

void setup() {

  delay(3000);

  Serial.begin(9600);

  Serial.println("Starting...");

  if (Ethernet.begin(mac) == 0) {

     Serial.println("Failed to configure Ethernet using DHCP");

  }

 

  delay(1000);

  Serial.println("connecting...");

 

  if (client.connect(server, 80)) {

      Serial.println("connected");

      client.println("http://www.xxx.NS1.php?P1=counter_value");

      client.println();

      Serial.println("Request sent");

  }

  else {

      Serial.println("connection failed");

  }

}

 

void loop()

{

}

 

Do you have an idea of what is wrong ?

Thanks for your help.

  • Sign in to reply
  • Cancel
Parents
  • benl
    benl over 14 years ago

    What is wrong is that you have to send an HTTP request, not a URL.

     

          client.println("http://www.xxx.NS1.php?P1=counter_value");

          client.println();

     

    should be

     

          client.print("GET /NS1.php?P1=counter_value HTTP/1.0\r\n");

           client.print("Host: xxx.xxx\r\n");

          client.print("\r\n");

     

    (println may do the right thing with the newlines, I don't know).




    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • benl
    benl over 14 years ago

    What is wrong is that you have to send an HTTP request, not a URL.

     

          client.println("http://www.xxx.NS1.php?P1=counter_value");

          client.println();

     

    should be

     

          client.print("GET /NS1.php?P1=counter_value HTTP/1.0\r\n");

           client.print("Host: xxx.xxx\r\n");

          client.print("\r\n");

     

    (println may do the right thing with the newlines, I don't know).




    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • fustini
    fustini over 14 years ago in reply to benl

    Ah ha, it was missing GET.  Nice catch!  I feel bad for not seeing that image   Hopefully this solves dakota77's issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to fustini

    Yes !

     

    It works fine now exactly with the 3 lignes suggested by Ben.

    Thanks a lot for your help