Arduino Forum Arduino Troubleshooting
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
  • Replies 7 replies
  • Subscribers 402 subscribers
  • Views 780 views
  • Users 0 members are here
  • mega
  • troubleshooting
  • trouble
  • troubleshoot
  • mega2560
  • arduino
  • arduino_mega
Related

Arduino Troubleshooting

dukeofmarshall
dukeofmarshall over 10 years ago

Good morning,

I am working on my first project and one of the things I am learning is interrupts. Specifically an interrupt from a button. I have connected up four LEDs on a breadboard to an Arduino Mega 2560. The sketch is simple enough. There are two patterns to light up the LEDs. One goes through each LED individually and the second pattern does both red LEDs at once and then switches to both green LEDs at once. Just something simple. I connected a button as an interrupt and this is meant to switch between patterns.

 

The basic premise works. The sketch starts out with one pattern and on the button push switches to the other pattern. However, the issue that I am running into is that after a short period one of the patterns gets "stuck" for some reason. You can view the issue in the video and the sketch is below as well as the serial output.

 

Another issue I am having is the initial serial output. For some reason the output is garbled and I have no idea why.

 

So is something wrong with the sketch or is there something possibly wrong with my Arduino? Thanks in advance for your time and advice.


You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

#define RED1 9

#define GREEN1 7

#define RED2 5

#define GREEN2 3

volatile int sequence = 0;

long last = 0;

volatile long last_used_millis = 0;

int delay_seconds = 1;

int sequence_number = 0;

 

 

void setup() {

  // put your setup code here, to run once:

    Serial.begin(9600);

    pinMode(RED1, OUTPUT);

    pinMode(RED2, OUTPUT);

    pinMode(GREEN1, OUTPUT);

    pinMode(GREEN2, OUTPUT);

    attachInterrupt(2, button, FALLING);

    Serial.println("Starting Program.............");

}

 

 

void loop() {

    int current_millis = millis();

 

    if(sequence == 1){

        if(current_millis - last_used_millis > (delay_seconds * 500)){

            switch(sequence_number){

                case 0:

                    digitalWrite(GREEN2, LOW);

                    digitalWrite(RED1, HIGH);

                    sequence_number = 1;

                    break;

                case 1:

                    digitalWrite(RED1, LOW);

                    digitalWrite(GREEN1, HIGH);

                    sequence_number = 2;

                    break;

                case 2:

                    digitalWrite(GREEN1, LOW);

                    digitalWrite(RED2, HIGH);

                    sequence_number = 3;

                    break;

                case 3:

                    digitalWrite(RED2, LOW);

                    digitalWrite(GREEN2, HIGH);

                    sequence_number = 0;

                    break;

            }

 

 

            last_used_millis = current_millis;

        }

    }else{

        if(current_millis - last_used_millis > (delay_seconds * 1000)){

            switch(sequence_number){

                case 0:

                    digitalWrite(GREEN1, LOW);

                    digitalWrite(GREEN2, LOW);

                    digitalWrite(RED1, HIGH);

                    digitalWrite(RED2, HIGH);

                    sequence_number = 1;

                    break;

                case 1:

                    digitalWrite(RED1, LOW);

                    digitalWrite(RED2, LOW);

                    digitalWrite(GREEN1, HIGH);

                    digitalWrite(GREEN2, HIGH);

                    sequence_number = 0;

                    break;

                default:

                    digitalWrite(GREEN1, LOW);

                    digitalWrite(GREEN2, LOW);

                    digitalWrite(RED1, HIGH);

                    digitalWrite(RED2, HIGH);

                    sequence_number = 1;

                    break;

            }

 

 

            last_used_millis = current_millis;

        }

    }

}

 

 

void button(){

    long current_millis = millis();

 

 

    if(current_millis - last > 1000){

        Serial.println("Button pressed");

 

 

        Serial.println("Current Millis is: "+String(current_millis));

        Serial.println("Last Millis is:    "+String(last));

        Serial.println("Difference is:     "+String(current_millis-last));

        if(sequence == 1){

            sequence = 0;

            Serial.println("Sequence 0");

        }else{

            sequence = 1;

            Serial.println("Sequence 1");

        }

        last = current_millis;

    }

}

 

Serial Output:

image

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 10 years ago

    A couple of questions:

    Are you using the default bootloader that comes with the board?

    Are you using the Arduino IDE to code with?

    If so, what version of the IDE are you using?

    Do you know what version of the AVR GCC compiler you're using?  This is assuming that you're, in fact, using the AVR GCC,

     

    I do notice that with at least I can see of the code you're not using one of the "Interrupts" libraries.  Obviously, I don't know if this was a conscious choice, or if you weren't aware of them.  I've occasionally seen where the AVR GCC doesn't use a destructor effectively (and sometimes not at all).  The ooPinChangeInt (and/or the arduino_pins, for the Atmega 128) library can make life easier.

     

    Most of the old problems with interrupts have been ironed out over time (and versions).  Some still crop up, however.  I wouldn't think this was a board problem, but someone with more expertise than myself might have a different opinion.  It would seem more like a memory leak that eventually crashes the programming.  I don't know how consistent the timing of the problem is (based upon that same number of state changes).  If the timing is fairly consistent then I'd assume it was a memory leak before thinking about a bad subckt on the chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 10 years ago

    A couple of questions:

    Are you using the default bootloader that comes with the board?

    Are you using the Arduino IDE to code with?

    If so, what version of the IDE are you using?

    Do you know what version of the AVR GCC compiler you're using?  This is assuming that you're, in fact, using the AVR GCC,

     

    I do notice that with at least I can see of the code you're not using one of the "Interrupts" libraries.  Obviously, I don't know if this was a conscious choice, or if you weren't aware of them.  I've occasionally seen where the AVR GCC doesn't use a destructor effectively (and sometimes not at all).  The ooPinChangeInt (and/or the arduino_pins, for the Atmega 128) library can make life easier.

     

    Most of the old problems with interrupts have been ironed out over time (and versions).  Some still crop up, however.  I wouldn't think this was a board problem, but someone with more expertise than myself might have a different opinion.  It would seem more like a memory leak that eventually crashes the programming.  I don't know how consistent the timing of the problem is (based upon that same number of state changes).  If the timing is fairly consistent then I'd assume it was a memory leak before thinking about a bad subckt on the chip.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dukeofmarshall
    dukeofmarshall over 10 years ago in reply to Former Member

    Default bootloader is being used.

    Arduino IDE is being used (1.6.5)

    AVR GCC? I have no clue. I can't even tell you what AVR GCC is right now.

     

    I didn't even know there were interrupt libraries. Seemed like a fairly basic and straightforward thing. I'll have to look more into that.