Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino Troubleshooting
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 407 subscribers
  • Views 815 views
  • Users 0 members are here
  • mega
  • troubleshooting
  • trouble
  • troubleshoot
  • mega2560
  • arduino
  • arduino_mega
Related

Arduino Troubleshooting

dukeofmarshall
dukeofmarshall over 10 years ago

Good morning,

I am working on my first project and one of the things I am learning is interrupts. Specifically an interrupt from a button. I have connected up four LEDs on a breadboard to an Arduino Mega 2560. The sketch is simple enough. There are two patterns to light up the LEDs. One goes through each LED individually and the second pattern does both red LEDs at once and then switches to both green LEDs at once. Just something simple. I connected a button as an interrupt and this is meant to switch between patterns.

 

The basic premise works. The sketch starts out with one pattern and on the button push switches to the other pattern. However, the issue that I am running into is that after a short period one of the patterns gets "stuck" for some reason. You can view the issue in the video and the sketch is below as well as the serial output.

 

Another issue I am having is the initial serial output. For some reason the output is garbled and I have no idea why.

 

So is something wrong with the sketch or is there something possibly wrong with my Arduino? Thanks in advance for your time and advice.


You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

#define RED1 9

#define GREEN1 7

#define RED2 5

#define GREEN2 3

volatile int sequence = 0;

long last = 0;

volatile long last_used_millis = 0;

int delay_seconds = 1;

int sequence_number = 0;

 

 

void setup() {

  // put your setup code here, to run once:

    Serial.begin(9600);

    pinMode(RED1, OUTPUT);

    pinMode(RED2, OUTPUT);

    pinMode(GREEN1, OUTPUT);

    pinMode(GREEN2, OUTPUT);

    attachInterrupt(2, button, FALLING);

    Serial.println("Starting Program.............");

}

 

 

void loop() {

    int current_millis = millis();

 

    if(sequence == 1){

        if(current_millis - last_used_millis > (delay_seconds * 500)){

            switch(sequence_number){

                case 0:

                    digitalWrite(GREEN2, LOW);

                    digitalWrite(RED1, HIGH);

                    sequence_number = 1;

                    break;

                case 1:

                    digitalWrite(RED1, LOW);

                    digitalWrite(GREEN1, HIGH);

                    sequence_number = 2;

                    break;

                case 2:

                    digitalWrite(GREEN1, LOW);

                    digitalWrite(RED2, HIGH);

                    sequence_number = 3;

                    break;

                case 3:

                    digitalWrite(RED2, LOW);

                    digitalWrite(GREEN2, HIGH);

                    sequence_number = 0;

                    break;

            }

 

 

            last_used_millis = current_millis;

        }

    }else{

        if(current_millis - last_used_millis > (delay_seconds * 1000)){

            switch(sequence_number){

                case 0:

                    digitalWrite(GREEN1, LOW);

                    digitalWrite(GREEN2, LOW);

                    digitalWrite(RED1, HIGH);

                    digitalWrite(RED2, HIGH);

                    sequence_number = 1;

                    break;

                case 1:

                    digitalWrite(RED1, LOW);

                    digitalWrite(RED2, LOW);

                    digitalWrite(GREEN1, HIGH);

                    digitalWrite(GREEN2, HIGH);

                    sequence_number = 0;

                    break;

                default:

                    digitalWrite(GREEN1, LOW);

                    digitalWrite(GREEN2, LOW);

                    digitalWrite(RED1, HIGH);

                    digitalWrite(RED2, HIGH);

                    sequence_number = 1;

                    break;

            }

 

 

            last_used_millis = current_millis;

        }

    }

}

 

 

void button(){

    long current_millis = millis();

 

 

    if(current_millis - last > 1000){

        Serial.println("Button pressed");

 

 

        Serial.println("Current Millis is: "+String(current_millis));

        Serial.println("Last Millis is:    "+String(last));

        Serial.println("Difference is:     "+String(current_millis-last));

        if(sequence == 1){

            sequence = 0;

            Serial.println("Sequence 0");

        }else{

            sequence = 1;

            Serial.println("Sequence 1");

        }

        last = current_millis;

    }

}

 

Serial Output:

image

  • Sign in to reply
  • Cancel
Parents
  • neilk
    neilk over 10 years ago

    Hi dukeofmarshall

     

    I think you need to look at this: https://www.arduino.cc/en/Reference/AttachInterrupt, which includes the following:

     

    "inside the attached function, delay() won't work and the value returned by millis() will not increment............... See the section on ISRs below for more information"

     

    I also followed the link labelled "Nick Gammon's Notes". Nick gives some simple rules about writing ISRs, including: "Don't Use Serial Prints"

     

    My own experience of using ISRs is to Set a flag inside the ISR and use the flag externally to indicate the need to execute a new section of code.

     

    Hope this helps

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • neilk
    neilk over 10 years ago

    Hi dukeofmarshall

     

    I think you need to look at this: https://www.arduino.cc/en/Reference/AttachInterrupt, which includes the following:

     

    "inside the attached function, delay() won't work and the value returned by millis() will not increment............... See the section on ISRs below for more information"

     

    I also followed the link labelled "Nick Gammon's Notes". Nick gives some simple rules about writing ISRs, including: "Don't Use Serial Prints"

     

    My own experience of using ISRs is to Set a flag inside the ISR and use the flag externally to indicate the need to execute a new section of code.

     

    Hope this helps

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dukeofmarshall
    dukeofmarshall over 10 years ago in reply to neilk

    Yeah, I was aware of the delay thing and that millis wouldn't increment. However, I thought that the process was moving through so fast that it wouldn't matter in an interrupt like that. Plus some of the examples that I ran across online for interrupts used pretty much the same process.

     

    So you think it might be with the Serial.println in the interrupt function?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • neilk
    neilk over 10 years ago in reply to dukeofmarshall

    hi dukeofmarshallHow about making your ISR as short as possible - eg do nothing apart from setting a flag to show that an interrupt has been received. Then in your main code - which is continually looping  - check the status of the flag and use that to decide whether or not to execute the code that currently sits in your ISR, remembering to clear the flag before you return to the main code.

     

    Hope this helps

     

    Neil