Arduino
  • Products
  • More
Arduino
Arduino Forum Relay sketch required for a charity project.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 417 subscribers
  • Views 1846 views
  • Users 0 members are here
Related

Relay sketch required for a charity project.

e14 Contributor
e14 Contributor over 14 years ago

A big hello from the UK!

 

I have a charity car project that is ongoing to raise funds for Help for Heroes. Our vehicle will be customised with lights, motors and sounds.

 

I have a standard arduino and a 4-relay board which is working well using various sketches I have found on the net.

 

I was wondering if anyone could help me with a sketch that will turn on 3, or 4 of these relays at a time interval that I can set from a single N/O momentery switch. I also need it to reset after a certain time so that when the button is pressed again the sequence will start again.

 

I have an HD44780 LCD that I'd like to work into the design that could display text just before the relevent relay becomes active. (This is not essential as the relays are my priority just now)

 

As it stands my relays, 1-4 are connected to pins 2-5 although I don't need the 4th relay at this time.

 

Basically the car will loosely resemble a helicopter and will have a set up of lights, motors and a cheap MP3 player that has a physical switch that when made instantly starts the helicopter sound file.

 

If I'm totally honest i think I need a 'pro' to write me a sketch that is really basic as I lack the skills to do it myself.

 

The lights, motors and mp3 will be powered externally and will be initiated with the arduino like this:

 

1. User presses a N/O momentery switch.

 

2. Relay 1 makes & MP3 plays, engine start up - and remains on for duration of file (1:52).

 

3. After 10 secs - Relay 2 makes and Navigation lights iluminate.

 

4. After engine warm-up 22secs relay 3 makes and 'rotors' start.

 

5. After 1:40 relay 3 breaks, rotors stop.

 

6. After 1:52 relays 1 & 2 break.

 

7. Next press of button, steps 1-6 start again.

 

If it is easier I can use a locking switch, would that would solve the re-set?

 

I know this is a big ask but i severely lack the programming knowledge to do this.

 

I hope someone can help, i'm sure it's not too difficult for you pros!

 

I really appreciate people reading this and taking the time to reply.

 

Many thanks in advance.

 

VB

  • Sign in to reply
  • Cancel

Top Replies

  • ntewinkel
    ntewinkel over 14 years ago +2
    Here we go. I had forgotten the 10k resistor to ground, so it took me a while to figure out why the button press was behaving so oddly! I tested using a momentary-on switch (gives 5 volts (high) when pressed…
  • ntewinkel
    ntewinkel over 14 years ago +1
    Challenge... accepted!
  • ntewinkel
    ntewinkel over 14 years ago in reply to e14 Contributor +1
    Hi Kris, I wrote it so that a line going HIGH means "ON", which I guess happens to be backwards To reverse that we just need to switch my HIGHs and LOWs wherever it says "digitalWrite(RELAY...". I just…
Parents
  • ntewinkel
    ntewinkel over 14 years ago

    Here we go. I had forgotten the 10k resistor to ground, so it took me a while to figure out why the button press was behaving so oddly!

    I tested using a momentary-on switch (gives 5 volts (high) when pressed), and 3 LEDs that go on when the pin goes HIGH.

     

    If anyone else wants to double check my work and/or give advice or tweaks, I welcome the input.

     

    /*

    Customized Vehicle with options, controlled by Arduino

    Written by Nico teWinkel

    www.mulBerryLand.com

    */

     

    // these are the pins the relays are connected to

    int RELAY1 = 2;

    int RELAY2 = 3;

    int RELAY3 = 4;

    //int RELAY4 = 5;

     

     

    // this is where the momentary switch is connected

    int STARTBUTTON = 8;

     

     

    // set up the start and stop times, in milliseconds

    // relay1 starts immediately

    long RELAY2_START_TIME = 10000;   // 0:10

    long RELAY3_START_TIME = 22000;   // 0:22

    long ACTION_STOP_TIME = 112000;  // 1:52    - stops relays 1 and 2

    long RELAY3_STOP_TIME = 100000;  // 1:40

     

     

    // this keeps track of the time since the button press

    long startTime;

    long lastTimeButtonPressed;

    long lastOutputTime;

     

     

    // active is TRUE when the actions are happening

    boolean active;

    boolean relay2_active;

    boolean relay3_active;

     

    void setup() {

      // start the serial for debug

      Serial.begin(9600);

      Serial.println("Starting application.");

     

      // set the relay pins as outputs

      pinMode(RELAY1, OUTPUT);

      pinMode(RELAY2, OUTPUT);

      pinMode(RELAY3, OUTPUT);

      //pinMode(RELAY4, OUTPUT);

     

      // set the pushbutton pin as an input

      pinMode(STARTBUTTON, INPUT);

     

      startTime = 0;

      active = false;

      relay2_active = false;

      relay3_active = false;

      lastTimeButtonPressed = -1000; // to avoid the initial 1 second button ignore

      lastOutputTime = 0;

    }

     

     

    void loop() {

     

     

      // check for button push

      // read the state of the switch into a local variable:

      int reading = digitalRead(STARTBUTTON);

     

      // ignore if button is pressed more than once per second

      // this also simplifies debounce

      if (millis() - lastTimeButtonPressed > 1000 && reading == HIGH) {

        lastTimeButtonPressed = millis();

        Serial.println("Button was pressed.");

       

        if (active) {

          // pushing the button when things are going on stops everything

          digitalWrite(RELAY1, LOW); // turn off relay1

          digitalWrite(RELAY2, LOW); // turn off relay2

          digitalWrite(RELAY3, LOW); // turn off relay3

          active = false;

        }

        else {

          active = true;

          startTime = millis();

          Serial.println("Turning ON relay 1");

          digitalWrite(RELAY1, HIGH); // turn on relay1

        }

      }

     

      if (active) {

        // show time once per second

        if((millis() - lastOutputTime) > 1000) {

          Serial.print("Time: ");

          Serial.println((millis() - startTime) / 1000);

          lastOutputTime = millis();

        }

       

        if (!relay2_active && millis() - startTime > RELAY2_START_TIME && millis() - startTime < ACTION_STOP_TIME) {

          Serial.println("Turning ON relay 2");

          digitalWrite(RELAY2, HIGH); // turn on relay2

          relay2_active = true;

        }

     

     

        if (!relay3_active && millis() - startTime > RELAY3_START_TIME && millis() - startTime < RELAY3_STOP_TIME) {

          Serial.println("Turning ON relay 3");

          digitalWrite(RELAY3, HIGH); // turn on relay3

          relay3_active = true;

        }

     

     

        if (relay3_active && millis() - startTime > RELAY3_STOP_TIME) {

          Serial.println("Turning OFF relay 3");

          digitalWrite(RELAY3, LOW); // turn off relay3

          relay3_active = false;

        }

     

     

        if (active && millis() - startTime > ACTION_STOP_TIME) {

          Serial.println("Turning OFF all relays");

          // stop everything

          // relay3 should already be off,

          //   but this makes sure it's all off in case there was a delay

          digitalWrite(RELAY1, LOW); // turn off relay1

          digitalWrite(RELAY2, LOW); // turn off relay2

          digitalWrite(RELAY3, LOW); // turn off relay3

          active = false;

          relay2_active = false;

          relay3_active = false;

        }

     

     

      }

     

    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ntewinkel
    ntewinkel over 14 years ago

    Here we go. I had forgotten the 10k resistor to ground, so it took me a while to figure out why the button press was behaving so oddly!

    I tested using a momentary-on switch (gives 5 volts (high) when pressed), and 3 LEDs that go on when the pin goes HIGH.

     

    If anyone else wants to double check my work and/or give advice or tweaks, I welcome the input.

     

    /*

    Customized Vehicle with options, controlled by Arduino

    Written by Nico teWinkel

    www.mulBerryLand.com

    */

     

    // these are the pins the relays are connected to

    int RELAY1 = 2;

    int RELAY2 = 3;

    int RELAY3 = 4;

    //int RELAY4 = 5;

     

     

    // this is where the momentary switch is connected

    int STARTBUTTON = 8;

     

     

    // set up the start and stop times, in milliseconds

    // relay1 starts immediately

    long RELAY2_START_TIME = 10000;   // 0:10

    long RELAY3_START_TIME = 22000;   // 0:22

    long ACTION_STOP_TIME = 112000;  // 1:52    - stops relays 1 and 2

    long RELAY3_STOP_TIME = 100000;  // 1:40

     

     

    // this keeps track of the time since the button press

    long startTime;

    long lastTimeButtonPressed;

    long lastOutputTime;

     

     

    // active is TRUE when the actions are happening

    boolean active;

    boolean relay2_active;

    boolean relay3_active;

     

    void setup() {

      // start the serial for debug

      Serial.begin(9600);

      Serial.println("Starting application.");

     

      // set the relay pins as outputs

      pinMode(RELAY1, OUTPUT);

      pinMode(RELAY2, OUTPUT);

      pinMode(RELAY3, OUTPUT);

      //pinMode(RELAY4, OUTPUT);

     

      // set the pushbutton pin as an input

      pinMode(STARTBUTTON, INPUT);

     

      startTime = 0;

      active = false;

      relay2_active = false;

      relay3_active = false;

      lastTimeButtonPressed = -1000; // to avoid the initial 1 second button ignore

      lastOutputTime = 0;

    }

     

     

    void loop() {

     

     

      // check for button push

      // read the state of the switch into a local variable:

      int reading = digitalRead(STARTBUTTON);

     

      // ignore if button is pressed more than once per second

      // this also simplifies debounce

      if (millis() - lastTimeButtonPressed > 1000 && reading == HIGH) {

        lastTimeButtonPressed = millis();

        Serial.println("Button was pressed.");

       

        if (active) {

          // pushing the button when things are going on stops everything

          digitalWrite(RELAY1, LOW); // turn off relay1

          digitalWrite(RELAY2, LOW); // turn off relay2

          digitalWrite(RELAY3, LOW); // turn off relay3

          active = false;

        }

        else {

          active = true;

          startTime = millis();

          Serial.println("Turning ON relay 1");

          digitalWrite(RELAY1, HIGH); // turn on relay1

        }

      }

     

      if (active) {

        // show time once per second

        if((millis() - lastOutputTime) > 1000) {

          Serial.print("Time: ");

          Serial.println((millis() - startTime) / 1000);

          lastOutputTime = millis();

        }

       

        if (!relay2_active && millis() - startTime > RELAY2_START_TIME && millis() - startTime < ACTION_STOP_TIME) {

          Serial.println("Turning ON relay 2");

          digitalWrite(RELAY2, HIGH); // turn on relay2

          relay2_active = true;

        }

     

     

        if (!relay3_active && millis() - startTime > RELAY3_START_TIME && millis() - startTime < RELAY3_STOP_TIME) {

          Serial.println("Turning ON relay 3");

          digitalWrite(RELAY3, HIGH); // turn on relay3

          relay3_active = true;

        }

     

     

        if (relay3_active && millis() - startTime > RELAY3_STOP_TIME) {

          Serial.println("Turning OFF relay 3");

          digitalWrite(RELAY3, LOW); // turn off relay3

          relay3_active = false;

        }

     

     

        if (active && millis() - startTime > ACTION_STOP_TIME) {

          Serial.println("Turning OFF all relays");

          // stop everything

          // relay3 should already be off,

          //   but this makes sure it's all off in case there was a delay

          digitalWrite(RELAY1, LOW); // turn off relay1

          digitalWrite(RELAY2, LOW); // turn off relay2

          digitalWrite(RELAY3, LOW); // turn off relay3

          active = false;

          relay2_active = false;

          relay3_active = false;

        }

     

     

      }

     

    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • billabott
    billabott over 14 years ago in reply to ntewinkel

    That is awesome.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 14 years ago in reply to ntewinkel

    I see I have a small bug that could keep relays2 and 3 off if the button was pressed to stop it before it was done.

    To fix that, add these 2 lines after "active = false;" in the if(active) block in the buttonpress block, to reset those relay status indicators:

     

          relay2_active = false;

          relay3_active = false;

     

    Hope the project goes well for you!

     

    Cheers,

    -Nico