Arduino
  • Products
  • More
Arduino
Arduino Forum Simple project for 10-11 year old.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 421 subscribers
  • Views 3433 views
  • Users 0 members are here
  • arduino_month
  • open-source
  • openhardware
  • lighting
  • diy
  • led
  • Design
  • platform
  • arduino_development_environment
  • engineering
  • electrical
  • arduino
  • opensource
Related

Simple project for 10-11 year old.

patkelly
patkelly over 14 years ago

I'm looking to do a project with some 10-11 year olds in a local school which uses electronics to show how they are feeling. I was thinking about a traffic light system where I can get the children to build the kit and then use it in under an hour. They would move the light to red when frustrated/mad and green for happy etc.

 

I have some of these Multicomp Nano boardsMulticomp Nano boards (1813414) which we can pre-program, and then add the rest of the part to it.

 

Any ideas would be greatfully received

 

Pat

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 14 years ago in reply to patkelly +1
    Did you ask the school if they would be okay with the students building lie detectors? I am opposed to knowledge suppression in all its forms. And your statement certainly set off my alarm bells. Okay…
  • YT2095
    YT2095 over 14 years ago in reply to patkelly +1
    if they`re going to be stand-alone boards, then a 9V batt and some clips would be an idea I also looked at those LEDs and from what I can see, I think you`ll need resistors for them, 330 Ohm or there abouts…
  • patkelly
    patkelly over 14 years ago in reply to billabott +1
    I second that, a massive thank you to Mr Nielsen, and everyone else who has contributed here I really can't believe the support you have all given on this.
Parents
  • dirtdiver
    dirtdiver over 14 years ago

    Hey that lie detector idea sounds interesting,

    the GSR detector is represented by two metal electrodes ?(any specific material?)

    The program does most of the work - have that gsr sensor as an analog input and read it a few times, get an average, and if it's over a certain point turn an led red?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dirtdiver
    dirtdiver over 14 years ago

    Hey that lie detector idea sounds interesting,

    the GSR detector is represented by two metal electrodes ?(any specific material?)

    The program does most of the work - have that gsr sensor as an analog input and read it a few times, get an average, and if it's over a certain point turn an led red?