Arduino
  • Products
  • More
Arduino
Arduino Forum arduino switching
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 417 subscribers
  • Views 832 views
  • Users 0 members are here
Related

arduino switching

e14 Contributor
e14 Contributor over 14 years ago

Seems easy / can it be done ?  want to input 64 momentry switches to toggle latch 64 outputs...any help appreciated

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    As long as you have enough 74HC595s to Shift Out and enough CD4021BEs to Shift In with then yes. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Would that be 8 of each ???  ............do you know if the arduino will interface with the 82C55 PIO chip by intercil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Yes 8 of each will give you 64 inputs and 64 outputs while only using 6 pin on the arduino.

     

    From what I can tell the 82C55 is a programmable interface chip. If you know how to use it then you can certainly use an Arduino to control it and its 24 i/o pins but you'll need to program the chip as well as the Arduino to control things. But I wouldn't know where to begin in wiring it to the arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Ok back to the 74 chips...Im ok with analog but dire with digital so excuse me !!

     

    Can I setup ,say, 20 memory stores where combinations of the switches can be saved and re-called.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thats doable. Its all in how you program the Arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 14 years ago in reply to e14 Contributor

    yes the 82C55 PIO should work with the arduino.  as for the memory stores that should also work.  ive attached and image that should help you with the wiringimage

    hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Nate1616
    Nate1616 over 14 years ago in reply to e14 Contributor

    yes the 82C55 PIO should work with the arduino.  as for the memory stores that should also work.  ive attached and image that should help you with the wiringimage

    hope this helps