Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum overheating resistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 422 subscribers
  • Views 4661 views
  • Users 0 members are here
  • help
  • overheating
  • arduino
  • relay
Related

overheating resistors

dirtdiver
dirtdiver over 14 years ago

Hi, im using the arduino to turn on a relay and complete a curcuit connecting the USB to a curcuit like this one :

 

    The IR's are TSHA203  , 100mA , Vr -5V, 180mW,image

Now one thig i dont understand is how 5 * 0.1 = 0.5 W and not 0.18 W, so I assumed that it could work on lower values like 2 volts or 50 mA and these are the maximum ones.

...But i guess i was wrong couse the resistors are overheating.Can you guys point me in the right direction?

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago +1
    You need to ask yourself "Do I need to drive with 100ma or not?". 100ma is the maximum non pulsed current allowed. As you already know, then the resistors need to dissipate about 500 mW. If the answer…
  • billabott
    billabott over 14 years ago +1
    Having watched this YouTube Video in order to learn what a "freetrack helmet" is; I have a suggestion in the form of a question. Why not use a single LED and 3 bundles of optical fiber(s)? These LEDs:…
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver +1
    interesting idea indeed, but if i use optical fiber first I would have to find optical fiber , http://www.mouser.com/Search/Refine.aspx?N=11203177
Parents
  • billabott
    billabott over 14 years ago

    Having watched this YouTube Video in order to learn what a "freetrack helmet" is; I have a suggestion in the form of a question.

     

    Why not use a single LED and 3 bundles of optical fiber(s)?

     

    These LEDs: 5mm Blue Water Clear Ultra Bright  that I buy from TaydaElectronics are rated as follows:

    Forward Voltage(V): 3.2-3.4   

    // three AAA rechargables are 3.6 volts /.: still need a resistor to drop ~0.3 volts
    Current(MA): 20
    View angle: 20 degrees   
    Luminous intensity(MCD): 12,000 - 18,000

    N.B.  Dividing that into three fiber bundles and you still have point sources in the range of 3000+ mcd each.

    If the camera being used can pick out the three points then that is what I will use when I build my Head Tracking unit using fiber bundles.  Hmm, now where to find them for cheap? Has anyone done any experiments with something like a RiteAV Digital Optical Toslink Cable 6ft ($2.36each)to see what kind point source you can get out of one cut in half?

    I MIGHT even hang the third point source from the chin strap just to be unique and assuming that the larger  triangle produces increase in angular resolution.  Probably will need to tell the software to flip the image upside down before processing OR write a modified driver.  image

     

    The Infrared LED  940nm 5mm TSAL7400

    Specifications are:
    Wave Length/Frequency: 940nm
    Product Type: Infrared LED
    Package: 5mm

     

    A fairly typical "bright" IR LED will put out about 27 mW/sr, though they go up to 250 mW/sr or so.  Source.

     

    For comparison the Red Water Clear LEDs made by Lite-On are only 1800 mcd @20mA.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • billabott
    billabott over 14 years ago

    Having watched this YouTube Video in order to learn what a "freetrack helmet" is; I have a suggestion in the form of a question.

     

    Why not use a single LED and 3 bundles of optical fiber(s)?

     

    These LEDs: 5mm Blue Water Clear Ultra Bright  that I buy from TaydaElectronics are rated as follows:

    Forward Voltage(V): 3.2-3.4   

    // three AAA rechargables are 3.6 volts /.: still need a resistor to drop ~0.3 volts
    Current(MA): 20
    View angle: 20 degrees   
    Luminous intensity(MCD): 12,000 - 18,000

    N.B.  Dividing that into three fiber bundles and you still have point sources in the range of 3000+ mcd each.

    If the camera being used can pick out the three points then that is what I will use when I build my Head Tracking unit using fiber bundles.  Hmm, now where to find them for cheap? Has anyone done any experiments with something like a RiteAV Digital Optical Toslink Cable 6ft ($2.36each)to see what kind point source you can get out of one cut in half?

    I MIGHT even hang the third point source from the chin strap just to be unique and assuming that the larger  triangle produces increase in angular resolution.  Probably will need to tell the software to flip the image upside down before processing OR write a modified driver.  image

     

    The Infrared LED  940nm 5mm TSAL7400

    Specifications are:
    Wave Length/Frequency: 940nm
    Product Type: Infrared LED
    Package: 5mm

     

    A fairly typical "bright" IR LED will put out about 27 mW/sr, though they go up to 250 mW/sr or so.  Source.

     

    For comparison the Red Water Clear LEDs made by Lite-On are only 1800 mcd @20mA.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dirtdiver
    dirtdiver over 14 years ago in reply to billabott

    interesting idea indeed, but if i use optical fiber first I would have to find optical fiber image , then im not sure that the web camera will be able to detect the fiber when the helmet is rotated , anyway i have the device ready and as soon as I find a visible light filter to put in front of the camera I will make a video

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    interesting idea indeed, but if i use optical fiber first I would have to find optical fiber image ,

    http://www.mouser.com/Search/Refine.aspx?N=11203177

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 14 years ago in reply to R_Phoenix

    The least expensive ones I have found are on Amazon.com and are known as Digital Audio Toslink Optical Cable (Toshiba Link).  Probably available at any high end audio store - maybe in their clearance bins.  I do remember something about when you cut a piece of fiber optic material - that it needs to be 'polished' so that the end 'face' is perpendicular to the light shaft media.  However, I am not sure exactly how to do that.