Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum overheating resistors
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 35 replies
  • Subscribers 422 subscribers
  • Views 4661 views
  • Users 0 members are here
  • help
  • overheating
  • arduino
  • relay
Related

overheating resistors

dirtdiver
dirtdiver over 14 years ago

Hi, im using the arduino to turn on a relay and complete a curcuit connecting the USB to a curcuit like this one :

 

    The IR's are TSHA203  , 100mA , Vr -5V, 180mW,image

Now one thig i dont understand is how 5 * 0.1 = 0.5 W and not 0.18 W, so I assumed that it could work on lower values like 2 volts or 50 mA and these are the maximum ones.

...But i guess i was wrong couse the resistors are overheating.Can you guys point me in the right direction?

Thanks!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago +1
    You need to ask yourself "Do I need to drive with 100ma or not?". 100ma is the maximum non pulsed current allowed. As you already know, then the resistors need to dissipate about 500 mW. If the answer…
  • billabott
    billabott over 14 years ago +1
    Having watched this YouTube Video in order to learn what a "freetrack helmet" is; I have a suggestion in the form of a question. Why not use a single LED and 3 bundles of optical fiber(s)? These LEDs:…
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver +1
    interesting idea indeed, but if i use optical fiber first I would have to find optical fiber , http://www.mouser.com/Search/Refine.aspx?N=11203177
  • dirtdiver
    dirtdiver over 14 years ago

    P.S. with the Vr=5V , so if that is the maxi Voltage , i wont need a resistor, so is it? image ..I cant even find the datasheet

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    Vr is reverse voltage max, and yes - you do need the resitor.

     

    I will assume the voltage drop of the Ir's is about 2 volts, so that leaves 3 volts droped across the resistor, so 3v / 30r = 100ma, 100ma * 3v = 300mw. What size are your resistors? For this they will need to be a half watt (half  500 mw and 1/4 is 250 mw). So I can see why they may be over heating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 14 years ago

    I agree with Phoenix in that you would need a half watt resistor.  2 volt drop across the IR is a good estimate since its usually between 1.6V to 2.2V.  hope this helps

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to R_Phoenix

    well my resistors are 0.25 W .. I will get 0.5 W tomorrow. thanks for the help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Nate1616
    Nate1616 over 14 years ago in reply to dirtdiver

    did upping the resistor wattage help you dirtdriver?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to Nate1616

    i just tried it with .5W and they are still verry hot.I just don't see the reason!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 14 years ago in reply to dirtdiver

    Curious, have you measured the voltage drop across the resistors and LEDs individually?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    Then you will need to accurately calculate the V drop (measure it with a meter) across the IR, and the Resistor. Each group should be close to the same. Then calculate the current draw of each to get the watts being dissipated by the resistors.

     

    quick calculations say that the v drop on the Ir should be around 1.7v so you should be using a 33 ohm resistor, but I bet a 100 ohm would work fine if you have some handy to try.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dirtdiver
    dirtdiver over 14 years ago in reply to R_Phoenix

    Each one should be the same? why?

    I measured it and its like this:

    image

    I gues the USB port isnt exactly 5 volts

    so 3.9 /30 = 130mA, 3.9*130=507mW

    oh man 7 mW above the max and the resistors are capable of cooking my dinner image

    its back to the store then..and again thanks for the help!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • R_Phoenix
    R_Phoenix over 14 years ago in reply to dirtdiver

    dirtdiver wrote:

     

    Each one should be the same? why?

    Each group, so each resitor should meassure 3.9 v drop, assumeing each resistor is identical. And each Ir should messure 1.7, again assuming they are the same values. IN your first drawing you have 3 in parallel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>