Arduino
  • Products
  • More
Arduino
Arduino Forum Hacking Power Supply
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 419 subscribers
  • Views 1376 views
  • Users 0 members are here
Related

Hacking Power Supply

billabott
billabott over 14 years ago

I am taking the plunge and building a Work Bench Power Supply from a PC Desktop power supply.

The guy in the video suggest that a approximate 0.5 amp load be put on the 5 volt rail (12 volt rail on newer) of the switching PS in order to stabilize it.

 

This diagram shows how he suggests putting it together.

 

What say you?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 14 years ago in reply to billabott +2
    Of the dozens of PC ATX-type power supplies I've used in analog, digital, and electrochemical circuits, I've never needed to add a "stabilizing" resistor. Basically, ground out the green wire, and the…
  • R_Phoenix
    R_Phoenix over 14 years ago +2
    The resistor isn't to stabilize the PSU, but rather give the system a dummy load on the 5v that helps "pull up" the 12. Taking the green wire to ground will still turn it on, but then messure the voltage…
  • terryking
    terryking over 14 years ago in reply to R_Phoenix +1
    Power resistors are hard to find. Just use a 12V Automotive tail light / side light bulb on the 5V supply. It will be bright enough to function as a "Pilot light" and will last almost forever at 5V...…
Parents
  • billabott
    billabott over 14 years ago

    image

     

    The one I have is HP part  number  5187-1098.  The OEM label says HIPRO HP-D2537F3R, 250 watts max. and there is a new part that replaces it designated HP part  number 5188-2622.  Mine has no burn smell and I only gave $1.10 for it.  image  Hope it is fully functional.

     

    I am thinking 22 ohm 10 watt (Newark Part Number 40M8806 @$0.55 each has NO Stock, I could go with 40M8183) might be the right fit.  Justification: (12 volts / 22 ohms) * 12 volts = 6.55 watts

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to billabott

    Of the dozens of PC ATX-type power supplies I've used in analog, digital, and electrochemical circuits, I've never needed to add a "stabilizing" resistor.

     

    Basically, ground out the green wire, and the fan comes on.  You get +12V on the yellow, +5V on the red, and GND on the black wires.  The whole setup requires one paper clip and about fifteen seconds with pliers.

     

    The thing I really love about PC power supplies is if you overload or short them, the crowbar circuit just kills the power with a quiet "zoop" sound.  It self-resets after about a minute, giving you time to reflect on electrical safety!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to billabott

    Of the dozens of PC ATX-type power supplies I've used in analog, digital, and electrochemical circuits, I've never needed to add a "stabilizing" resistor.

     

    Basically, ground out the green wire, and the fan comes on.  You get +12V on the yellow, +5V on the red, and GND on the black wires.  The whole setup requires one paper clip and about fifteen seconds with pliers.

     

    The thing I really love about PC power supplies is if you overload or short them, the crowbar circuit just kills the power with a quiet "zoop" sound.  It self-resets after about a minute, giving you time to reflect on electrical safety!