Arduino Forum One Wire temp Question
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
  • Replies 7 replies
  • Subscribers 394 subscribers
  • Views 492 views
  • Users 0 members are here
Related

One Wire temp Question

Former Member
Former Member over 12 years ago

Hey all, im new to arduino, excited and ready to get roaing into my projects, but im a little stuck at the moment.

 

Using the dallas temp sensors ds18b20, i want to display the output on an lcd screen, which seems fine however i dont want for example :

 

35.xx , i only require the main temp 35 not requiring the display of the decimal point, is there any way for me to configure this ?

 

please keep in mind im pretty new to all the code, so im trying to get my head around that.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1
    as a simple measure without getting into casts etc, use the printf function or sprintf found in STDIO.H or printf.h printf("'%.2f'", 10.3456); // prints to two decimal places (10.35) printf("'%.0f'", 10…
  • mconners
    mconners over 12 years ago

    I'd really have to see your code to know exactly what you are doing, but from the description, you could just cast the double/float or whatever to an int to get just the integral part of the temp reading. I'm sure if you posted the code you could get a better response.

     

    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • chgus
    chgus over 12 years ago

    The int() function comes to mind ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago

    ahhhh, got it, thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billpenner
    billpenner over 10 years ago in reply to mconners

    In in your reply to Michael Conners. Please explain what " cast the double/float " means and how to do it. I am trying to learn and this will help me in a project.

    Thanks,

    Bill

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to billpenner

    Hi billpenner.

     

    This page should clarify the cast operator for you: Arduino - Cast

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • billpenner
    billpenner over 10 years ago in reply to gadget.iom

    I see. It looks like a cast is a translation from one type to another.

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    as a simple measure without getting into casts etc, use the printf function or sprintf found in STDIO.H or printf.h


    printf("'%.2f'", 10.3456); // prints to two decimal places (10.35)

    printf("'%.0f'", 10.3456); // prints to no decimal places (10)


    or

    char str[] = "hello this is my current buffer with this string in it";

    sprintf(str, "Happy New Year: %s ", stringtoinsert); // inserts string into buffer "str" at the place indicated by %s

     

    then you can use the str variable to print like this

    Serial.print(str);

     

    or LCD.print(str);

     

    as you can see more flexible than the printf() which only prints to console

     

    there both formatting directives, the printf directly prints the string to console, the sprintf updates a character array with the formatted string

     

    the formatting for each is the same and is detailed here :http://www.cplusplus.com/reference/cstdio/printf/

     

    Hope this helps to give you more options

    Peter