Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino mega 2560 powering lots of 5V relays.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 416 subscribers
  • Views 393 views
  • Users 0 members are here
Related

Arduino mega 2560 powering lots of 5V relays.

e14 Contributor
e14 Contributor over 13 years ago

Hi, everybody. I'm new here and have just bought an Arduino mega 2560.  I wonder how many dpdt 5v relays I can power directly from the Arduino mega 2560?If I use DPDT relays, I probably can do what i need with 10 relays. (I.e. 10 binary bits).

 

Thx for the help.

 

Luke

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 13 years ago

    I depends on the current the relays require when operated.

     

    It's best if you look at using a seperate supply for the relay coils.

    If you used optocoupled relays, you could then use 12v, which would also feed into the Vin of the mega.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 13 years ago

    I depends on the current the relays require when operated.

     

    It's best if you look at using a seperate supply for the relay coils.

    If you used optocoupled relays, you could then use 12v, which would also feed into the Vin of the mega.

     

     

    Mark