Arduino
  • Products
  • More
Arduino
Arduino Forum trying to get an LED to come on for 3 seconds and come off without delay
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 420 subscribers
  • Views 7442 views
  • Users 0 members are here
  • arduino_code
Related

trying to get an LED to come on for 3 seconds and come off without delay

e14 Contributor
e14 Contributor over 13 years ago

hey guys i'm just trying to get an led to come on for 3 seconds and then comeoff, without using delay, i'm not understanding the millis function but i've tried a bit. kindly let me know what i'm doing wrong. thank you.

 

int count = 0;
long previousMillis = 0;        




long interval = 3000;           


void setup() {
  // set the digital pin as output:
  pinMode(ledPin, OUTPUT);    
  
}


void loop()
{
  
  unsigned long currentMillis = millis();

  if(currentMillis - previousMillis > interval) {
    
    previousMillis = currentMillis;   


     if (count <=1)
      digitalWrite(ledPin,HIGH);
    else
      digitalWrite(ledPin,LOW);
count ++;
    
    
  }
}

  • Sign in to reply
  • Cancel

Top Replies

  • billabott
    billabott over 13 years ago in reply to phoenixcomm +2
    Interesting insight Cris H. Unfortunately, your code does not plug into the 'Duino IDE too well. So, I took some time to create my own completely commented version which I now make available to everyone…
  • ntewinkel
    ntewinkel over 13 years ago in reply to e14 Contributor +1
    To have red and green alternating on, you basically copy the lines of code that turn the ledpin high and low and set opposite values for the other LED. ie, when you turn the red led on, at that time you…
  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Thank you Navin and Nico I will definately try out the two versions! You guys are awesome and I will give you 50 cool points each! Seriously though, I just wish I could one day be as helpful as you two…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Thank you Navin and Nico I will definately try out the two versions! You guys are awesome and I will give you 50 cool points each! image Seriously though, I just wish I could one day be as helpful as you two are, I am still trying to figure the whole IDE language and there are a plethora of books out there. I am super lost as to where to start. Bah!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • billabott
    billabott over 13 years ago in reply to e14 Contributor
    This reply was deleted.
    • Cancel
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to billabott

    billabott wrote:

     

    Well, I can tell you and everyone else that the place to start is here: http://www.amazon.com/Programming-Language-2nd-Brian-Kernighan/dp/0131103628/ref=la_B000AQ1TNQ_1_1?ie=UTF8&qid=1364699822&sr=1-1

     

    It's such a great book. Ultra-concise and to the point. And although it is expensive compared to others, it holds it's value well and you can always sell it if you ever decide you don't need it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 13 years ago in reply to billabott

    billabott wrote:

     

    Well, I can tell you and everyone else that the place to start is here: http://www.amazon.com/Programming-Language-2nd-Brian-Kernighan/dp/0131103628/ref=la_B000AQ1TNQ_1_1?ie=UTF8&qid=1364699822&sr=1-1

     

    It's such a great book. Ultra-concise and to the point. And although it is expensive compared to others, it holds it's value well and you can always sell it if you ever decide you don't need it.