Arduino
  • Products
  • More
Arduino
Arduino Forum making mosquito high frequency to repel
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 420 subscribers
  • Views 4713 views
  • Users 0 members are here
Related

making mosquito high frequency to repel

e14 Contributor
e14 Contributor over 13 years ago

I was hoping to get advice on how to  generates high frequency sound that may repel mosquitoes.

 

Any ideas on this project ???

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to groaker +2
    Dont let someone else's failure hold you back. Give it a shot. you may want to ry different frequencies or multiple frequencies.High, higher, or lower. Give it a try.
  • groaker
    groaker over 13 years ago +1
    A number of studies have demonstrated that high frequency sounds do not repel mosquitos. This bit of folklore probably came about between the presence of bats, of which some species are prodigious eaters…
  • michaelkellett
    michaelkellett over 13 years ago in reply to e14 Contributor +1
    @chinino Why, in the face of evidence to the contrary, are you so convinced that some noise at some high frequency will upset mosqitos. ? Here is a link to supplement Michael Tria's post. http://www.bbc…
Parents
  • ntewinkel
    ntewinkel over 13 years ago

    I don't know if a piezo speaker/buzzer gets you the right frequencies, but here is an example circuit from Oomlout to make sound:

    http://www.oomlout.com/oom.php/products/ardx/circ-06

     

    For the high frequencies, maybe keep an eye on nearby dogs and cats when testing - they can hear up to something like 65-85KHz.

     

    And I guess you can do testing with a few pop-bottle and yeast mosquito traps (one with your repeller, the other without) - that's assuming those traps work image

     

    Good luck, hope it works out!

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to ntewinkel

    Did not see any specs on FreQ range on oomlout.

     

     

     

    Will need a High Freq speakers but also may have to test with lower freq.  I think some type of noise will repel them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 13 years ago in reply to e14 Contributor

    That Oomlout example is only showing how to hook up a piezo speaker/buzzer and gives a very basic example of how to make some tones, but you can modify the code to get to your desired frequency. Look at their comments for notes, for example:

    * note      frequency      period      timeHigh

    * c     261 Hz     3830      1915 

     

    I'm guessing that changing timeHigh to 19 would give you close to 26,100 Hz, or 26 kHz.

     

    You'd have to do some math to figure out the required delays to get the desired frequencies (smaller delay = higher frequency), but the rest is pretty much there for you to use.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 13 years ago in reply to e14 Contributor

    @chinino

     

    Why, in the face of evidence to the contrary, are you so convinced that some noise at some high frequency will upset mosqitos. ?

     

    Here is a link to supplement Michael Tria's post.

     

    http://www.bbc.co.uk/news/magazine-20669080

     

    Before you start trying to make any noise try to find some research results that indicate what sort of noise might be effective.

    If you can find any then post a link here I'll be very happy to advise you about how to generate the sounds.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • groaker
    groaker over 13 years ago in reply to michaelkellett

    There are people who want to believe that the Second Law of Thermodynamics can be violated. That the circle can be squared. That there is a map that need more than four colors. That even though the flu vaccine is a killed vaccine, that it will give them the flu.

     

    Most of the time such antics keep them busy, and out of harms way. Sometimes, like Andrew Wakefield and the phony MMR-autism link, they do real damage, and kill thousands. Looking for some fx that will frighten away mosquitos is a relatively harmless though fruitless pastime.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • groaker
    groaker over 13 years ago in reply to michaelkellett

    There are people who want to believe that the Second Law of Thermodynamics can be violated. That the circle can be squared. That there is a map that need more than four colors. That even though the flu vaccine is a killed vaccine, that it will give them the flu.

     

    Most of the time such antics keep them busy, and out of harms way. Sometimes, like Andrew Wakefield and the phony MMR-autism link, they do real damage, and kill thousands. Looking for some fx that will frighten away mosquitos is a relatively harmless though fruitless pastime.