Arduino
  • Products
  • More
Arduino
Arduino Forum making mosquito high frequency to repel
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 420 subscribers
  • Views 4719 views
  • Users 0 members are here
Related

making mosquito high frequency to repel

e14 Contributor
e14 Contributor over 13 years ago

I was hoping to get advice on how to  generates high frequency sound that may repel mosquitoes.

 

Any ideas on this project ???

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to groaker +2
    Dont let someone else's failure hold you back. Give it a shot. you may want to ry different frequencies or multiple frequencies.High, higher, or lower. Give it a try.
  • groaker
    groaker over 13 years ago +1
    A number of studies have demonstrated that high frequency sounds do not repel mosquitos. This bit of folklore probably came about between the presence of bats, of which some species are prodigious eaters…
  • michaelkellett
    michaelkellett over 13 years ago in reply to e14 Contributor +1
    @chinino Why, in the face of evidence to the contrary, are you so convinced that some noise at some high frequency will upset mosqitos. ? Here is a link to supplement Michael Tria's post. http://www.bbc…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    i will send a sch to do and change the capacitor to set right value to your frequency to block out mosquitos

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ChuckMcM
    ChuckMcM over 13 years ago in reply to e14 Contributor

    This has been a fun thread. Generally it's accepted that mostquitos are not repelled by high frequencies, however at enough sound pressure you could no doubt damage them! :-) That said, there are lots of fun things you can do an ultrasonic speaker, and a system for generating various frequencies. (and it does annoy dogs so be ready for them to 'sing along' :-) One of my favorites is to take two ultrasonic speakers and have them emit a sinusoid at the same frequency (say 30kHz to be safely out of most people's hearing). Then set them up in a room pointing at different walls. This will create a bunch of standing waves where the sounds overlap.

     

    Now frequency modulate one the speakers with a recognizable audio signal and walk around the room. What you will hear are pockets where the audio is very clear and seems to "spring" right out of the air. Its very creepy and great for a seance party. Other fun things you can do are create air cavities in a 2-liter bottle and set them on a counter, modulate the frequency until you find the resonant frequency of the bottle cavity. Great fun to watch the bottles jump around.

     

    Needless to say, you will be having so much fun you will forget all about the mosquitos.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ChuckMcM
    ChuckMcM over 13 years ago in reply to e14 Contributor

    This has been a fun thread. Generally it's accepted that mostquitos are not repelled by high frequencies, however at enough sound pressure you could no doubt damage them! :-) That said, there are lots of fun things you can do an ultrasonic speaker, and a system for generating various frequencies. (and it does annoy dogs so be ready for them to 'sing along' :-) One of my favorites is to take two ultrasonic speakers and have them emit a sinusoid at the same frequency (say 30kHz to be safely out of most people's hearing). Then set them up in a room pointing at different walls. This will create a bunch of standing waves where the sounds overlap.

     

    Now frequency modulate one the speakers with a recognizable audio signal and walk around the room. What you will hear are pockets where the audio is very clear and seems to "spring" right out of the air. Its very creepy and great for a seance party. Other fun things you can do are create air cavities in a 2-liter bottle and set them on a counter, modulate the frequency until you find the resonant frequency of the bottle cavity. Great fun to watch the bottles jump around.

     

    Needless to say, you will be having so much fun you will forget all about the mosquitos.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 13 years ago in reply to ChuckMcM

    Chuck

     

    That frequency modulating seems to be the method used for the range of speakers that are highly directional.

    http://www.holosonics.com/ is one of a few around.

     

    Must remember this trick for another day.

     

    Thanks

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to mcb1

    So as any one confirmed or otherwise the fact that our insect friends are discouraged by the ultrasound?

    To be hoest I'm not even sure about the rodents, I know that Dogs don't like it and do start barking which isn't what you realy want I'm sure.:)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 13 years ago in reply to Problemchild

    John

    I think the article that was linked to tended to suggest that they weren't discouraged.

    However there are some that still think there is something the tests missed ....

     

    Of course the spray companies would love to continue selling, so anything that is a one time purchase is not in their interest.

     

    Rodents are probably like Dogs and Cats especially since they do use hearing to good effect and have similar ear structures (on the outside anyway), and are likely to NOT like ultrasonics.

    If anyone thinks I'm wrong about mosquitoes and hearing, please send me a picture showing those large ears that are able to be turned ....

     

    Not that we have mosquito issues, but we use one of the feramone auto sprayers to keep the smaller flies outside, and that works well.

     

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to mcb1

    Thinking about it I remember ones that DX.com sold that claimed to work because they sounded similar to the male mosquito and this kept others away.

     

    To be honest this circuit is so simple then you would be best not to belive any one but to try it out..

    It would make a good project and video image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to Problemchild

    How about going to Pat Kelly's page and putting an idea on this now very long LPC800 thread

     

    http://www.element14.com/community/docs/DOC-54622#comment-24214

     

    Get a free dev board from them and put the amp and speaker on it. You can easily vary and experiment withe the output frequencies with your free Swag !!

     

     

     

    Vive over engineering!!