Arduino
  • Products
  • More
Arduino
Arduino Forum First arduino project, please help.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 418 subscribers
  • Views 743 views
  • Users 0 members are here
Related

First arduino project, please help.

e14 Contributor
e14 Contributor over 13 years ago

Ok, so i started a project utilizing arduinos (2x) (havent decided to go uno or mega yet)

 

My quesion is while using a tft screen and an adapter shield is there any way to expand the board?

I have ran out of pins. my project requires 15 output pins and 5 input pins(some analog and some digital) other than what are being used buy the tft screens.

 

is there anyway to make 2 or 3 arduino boards communicate with eachother instantly?

 

example: if arduino board(1) reads a digital signal into pin 5

              then arduino board(2) reads that arduino board(1) has recieved the signal so it sends a 5v output to a relay via pin 8?

 

I have yet to purchace my arduino boards, I would like some input about what would be the best way to do this.

 

Any help would be greatly appreciated, Thank You.

  • Sign in to reply
  • Cancel
Parents
  • alanwood
    alanwood over 13 years ago

    Hi Anthony,

     

    The Arduino Mega should fulfil your requirements.

     

    The site quotes "The Arduino Mega is a microcontroller board based on the ATmega1280. It has 54 digital input/output pins (of which 14 can be used as PWM outputs), 16 analog inputs, 4 UARTs (hardware serial ports), a 16 MHz crystal oscillator, a USB connection, a power jack, an ICSP header, and a reset button."

     

    This should leave plenty of I/O after the shields are fitted. Can you let us know which TFT and adaptor shields you are using please?

     

    Have fun!

     

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • alanwood
    alanwood over 13 years ago

    Hi Anthony,

     

    The Arduino Mega should fulfil your requirements.

     

    The site quotes "The Arduino Mega is a microcontroller board based on the ATmega1280. It has 54 digital input/output pins (of which 14 can be used as PWM outputs), 16 analog inputs, 4 UARTs (hardware serial ports), a 16 MHz crystal oscillator, a USB connection, a power jack, an ICSP header, and a reset button."

     

    This should leave plenty of I/O after the shields are fitted. Can you let us know which TFT and adaptor shields you are using please?

     

    Have fun!

     

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to alanwood

    Thank you for your response, Alan.

     

    The below linked is the tft screen that i have picked i will be running 2 of them unless i can find a decent 5" screen then ill just run that

     

    http://www.colorapples.com/32-tft-lcd-screen-module-p-88877.html#.UflbFI1ONic

     

    And, the below link is the before said tft adapter shield.

     

    http://www.ebay.com/itm/TFT-SD-Shield-for-Arduino-DUE-TFT-LCD-Module-SD-Card-Adapter-2-8-3-2-inch-Mega-/121057447668?pt=LH_DefaultDomain_0&hash=item1c2f960ef4

     

    Idk if it is needed to have the sd card slot to pull graphics off of i just assumed that would be easiest on the board.

     

    this project will be running a good portion of my project car. including; blinkers, enigne on\off, heater controls, vent controls, hazard lights, windows, defrost defog, and other misc things around the vehicle. quite a big project but willing to put the time and effort into making it work.