Arduino
  • Products
  • More
Arduino
Arduino Forum First arduino project, please help.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 418 subscribers
  • Views 743 views
  • Users 0 members are here
Related

First arduino project, please help.

e14 Contributor
e14 Contributor over 13 years ago

Ok, so i started a project utilizing arduinos (2x) (havent decided to go uno or mega yet)

 

My quesion is while using a tft screen and an adapter shield is there any way to expand the board?

I have ran out of pins. my project requires 15 output pins and 5 input pins(some analog and some digital) other than what are being used buy the tft screens.

 

is there anyway to make 2 or 3 arduino boards communicate with eachother instantly?

 

example: if arduino board(1) reads a digital signal into pin 5

              then arduino board(2) reads that arduino board(1) has recieved the signal so it sends a 5v output to a relay via pin 8?

 

I have yet to purchace my arduino boards, I would like some input about what would be the best way to do this.

 

Any help would be greatly appreciated, Thank You.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Also wondering if i use the rx tx serial pins. if i have the touchscreen arduino send a certain integer if the other arduino can read that integer and perform an action.

     

    example:

    Touch arduino: Press button"1" on the screen. send a "1" through the tx pin

     

    Second arduino: Recieves the "1" and sends power to pin 8

     

    Touch arduino: Press button "2" on the screen. send a "2" through the tx pin

     

    Second arduino: Recieves the "2" and sends power to pin 10

     

     

    I understand that probably wont support any multi touch function. but im not really aiming for that. lol.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • alanwood
    alanwood over 13 years ago in reply to e14 Contributor

    Hi Anthony,

     

    Thanks for the info. I'm having a bit of a think...

     

    If anyone else has ideas, please chip in as I'm fairly new to Arduino myself!

     

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • alanwood
    alanwood over 13 years ago in reply to e14 Contributor

    Hi Anthony,

     

    Thanks for the info. I'm having a bit of a think...

     

    If anyone else has ideas, please chip in as I'm fairly new to Arduino myself!

     

    Alan