Arduino
  • Products
  • More
Arduino
Arduino Forum robotic wheel chair help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 420 subscribers
  • Views 3309 views
  • Users 0 members are here
Related

robotic wheel chair help

e14 Contributor
e14 Contributor over 12 years ago

can some one help me with robotic wheel chair using arduino uno

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 12 years ago in reply to rajiv.tctech +1
    The ESP article is OK as far as it goes but it's really only concerned with simple mains power supplies. It has a tiny section at the end about switching supplies but it's way out of date. The wheelchair…
  • alanwood
    alanwood over 12 years ago in reply to e14 Contributor +1
    Hi Prajwal, This is supposed to be your project not ours. If you keep asking questions and expecting answers, you will never learn how to be an engineer. That is why you are training, isn't it? I'm sorry…
Parents
  • rajiv.tctech
    rajiv.tctech over 12 years ago

    Prajwal, broadly you need to do the following:

     

    1. Read an analog 2-axis joystick with the Arduino analog input ports. The magnitude and direction of the X-axis input of the joystick should output a differential PWM output to the left and right DC motor H-Bridge amplifiers which is applied to the PWM duty-cycle worked out in point 2 below.

    2. The Y-axis input of the joystick should control the duty-cycle of the PWM, i.e. the speed of the wheelchair.

    3. There should be an Emergency Stop switch, easily accessible by the user of the wheelchair.

    4 Steering will be effected by using caster wheels in front and differential drive to left and right motors ( Point 1 above)

    5. You may also want to examine raising and lowering the chair with an up/down selector, to empower the wheelchair user in raising him/her to the height of upright bipedal people.

     

    Before you actually allow a differently abled person to use the wheelchair, you will need to examine safety features like over-riding the system if it begins to misbehave due to faulty input from the joystick. Please ensure you use a WDT (watch dog timer) system to check that your processor has not locked up with a certain output.

     

    Rajiv

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rajiv.tctech
    rajiv.tctech over 12 years ago

    Prajwal, broadly you need to do the following:

     

    1. Read an analog 2-axis joystick with the Arduino analog input ports. The magnitude and direction of the X-axis input of the joystick should output a differential PWM output to the left and right DC motor H-Bridge amplifiers which is applied to the PWM duty-cycle worked out in point 2 below.

    2. The Y-axis input of the joystick should control the duty-cycle of the PWM, i.e. the speed of the wheelchair.

    3. There should be an Emergency Stop switch, easily accessible by the user of the wheelchair.

    4 Steering will be effected by using caster wheels in front and differential drive to left and right motors ( Point 1 above)

    5. You may also want to examine raising and lowering the chair with an up/down selector, to empower the wheelchair user in raising him/her to the height of upright bipedal people.

     

    Before you actually allow a differently abled person to use the wheelchair, you will need to examine safety features like over-riding the system if it begins to misbehave due to faulty input from the joystick. Please ensure you use a WDT (watch dog timer) system to check that your processor has not locked up with a certain output.

     

    Rajiv