Arduino
  • Products
  • More
Arduino
Arduino Forum robotic wheel chair help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 30 replies
  • Subscribers 420 subscribers
  • Views 3287 views
  • Users 0 members are here
Related

robotic wheel chair help

e14 Contributor
e14 Contributor over 12 years ago

can some one help me with robotic wheel chair using arduino uno

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 12 years ago in reply to rajiv.tctech +1
    The ESP article is OK as far as it goes but it's really only concerned with simple mains power supplies. It has a tiny section at the end about switching supplies but it's way out of date. The wheelchair…
  • alanwood
    alanwood over 12 years ago in reply to e14 Contributor +1
    Hi Prajwal, This is supposed to be your project not ours. If you keep asking questions and expecting answers, you will never learn how to be an engineer. That is why you are training, isn't it? I'm sorry…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    how can i control the speed of dc motors using the same joystick...pls help me...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rajiv.tctech
    rajiv.tctech over 12 years ago in reply to e14 Contributor

    The left right movement of the joystick can be used to steer the wheelchair by differentially driving the wheels. The Y-axis of the joystick, or say the forward and back motion of the joystick can be used to vary speed and direction - pulling the joystick back from the centre-point could make the motors reverse direction. But in all this, do remember to keep a deadband around the centre-point of the joystick, wherein the values do not do anything. Otherwise you might land up with a wheelchair that keeps creeping even without any control input...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rajiv.tctech
    rajiv.tctech over 12 years ago in reply to e14 Contributor

    The left right movement of the joystick can be used to steer the wheelchair by differentially driving the wheels. The Y-axis of the joystick, or say the forward and back motion of the joystick can be used to vary speed and direction - pulling the joystick back from the centre-point could make the motors reverse direction. But in all this, do remember to keep a deadband around the centre-point of the joystick, wherein the values do not do anything. Otherwise you might land up with a wheelchair that keeps creeping even without any control input...