Arduino
  • Products
  • More
Arduino
Arduino Forum Can someone explain how this V-USB circuit works?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 420 subscribers
  • Views 2446 views
  • Users 0 members are here
  • v-usb
  • usb
  • Design
  • attiny
  • arduino
  • vusb
Related

Can someone explain how this V-USB circuit works?

e14 Contributor
e14 Contributor over 12 years ago

Hi everyone,

 

http://www.practicalarduino.com/pics/virtual-usb-keyboard-schematic.jpg

I'm attempting to learn how to communicate with Atmel chips such as the Attiny85 without having to use a serial-to-USB converter. I'm fairly new to electronics circuit design, and I am having trouble understanding what role the zener diodes and resistors have in the communication between the 5V MCU and USB. If you can, please explain why certain resistances and zener diode ratings are used in this situation(and why zener diodes work and regular diodes don't)

 

Thanks in advance,

Tom

  • Sign in to reply
  • Cancel
  • deltalat
    deltalat over 12 years ago

    Tom,

     

    The difference between a zener diode and a plane old vanilla diode is that a zener will break down and conduct current when a reverse voltage exceeds a threshold. In your diagram, if we drive DIO2 with a voltage > 3.6 volts, then the zener will turn on limiting D-/D+ to ~3.6 V.

    The 68 ohm resistors will help to limit the amount of current flowing through the reversed biased diode. If we are driving the signal with 5V, then the current thought the zener will be limited to approximately 20 mA. In addition, the resistors will help slow the output signal down a bit, decreasing ringing/emi/etc.

    The 2.2k DIO5 resistor probably is used to indicate a low speed usb device.

     

    Best Regards,

     

    Argus

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to deltalat

    Will it work with a 100 ohm resistor instead of the 68 ohm? I just bought this Attiny85 and I have some spare resistors to try it but I am not sure if 100 ohms will work the same as I don't have any 68 ohm.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    It wont be ideal but should work if wiring is short, so if your doing this on a breadboard or similar then it should be ok (Functional)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to Robert Peter Oakes

    @Tom

     

    For a quick lash up there is no need to worry about the zeners (except that you probably don't need them at all.)

     

    The usual reason for adding some kind of voltage clamping to USB data lines is to ensure that they will pass EMC testing. One of the tests is to apply high voltage discharges to the signal lines to simulate the kind of thing that will happen if you touch one with a finger while you are carrying  a static charge. In dry conditions with some kinds of carpet this can happen often. Test specs vary but typically you might expect to apply 8kV from a 100pF capacitor via a 1500ohm resistor (simulated Human Body Discharge Human-body model - Wikipedia, the free encyclopedia) . The initial current into your USB line will be about 5.3A and a typical 3.6V 400mW zener will have a dynamic resistance of about 24ohms so the voltage across the zener will rise to over 100V (in real life it might not be quite so bad because of the zener's self capacity). Zeners are no use in this application. There are lots of transient protection devices available which WILL clamp the HBD but they don't work very well without careful pcb layout - on breadboard just don't bother.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 12 years ago

    The designer would have been better served to split his input resistors and place his Zeners at the taps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to D_Hersey

    Not really !

     

    USB chips vary a little but usually need series resistors between zero and 22 ohms. Splitting these doesn't help much - 100V on the zener and 10ohms from that to the chip still makes a dead chip. A big series R would protect the chip nicely but the USB spec can't be met with much more R than the chip supplier recommends and it won't work at all with much more than 100R. You can see one of many better ways to do it here: http://arduino.cc/en/uploads/Main/arduino-uno-schematic.pdf

    (But you won't easily find the devices they refer to so you would need to poke around to find substitutes.)

     

    I would use one of these, you need a board and it's surface mount but ESD protection doesn't really work any other way so nothing is lost:

     

     

    STMICROELECTRONICS - USBLC6-2P6 - DIODE ARRAY, TVS, USB2

     

     

    STMICROELECTRONICSUSBLC6-2P6
    Image is for illustrative purposes only.
    Please refer to product description

     

    Manufacturer:
    STMICROELECTRONICS
    Order Code:
    1295310
    Manufacturer Part No:
    USBLC6-2P6

     

    Technical Data Sheet (219.00KB) EN
    Technical Data Sheet (219.00KB) EN

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago

    I suggest you head over to the Digispark forums.

    They use this method and Bluebie has some very good explanations of it.

     

    There are also some explanations of programming raw chips.

     

    Mark