Arduino
  • Products
  • More
Arduino
Arduino Forum Can someone explain how this V-USB circuit works?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 420 subscribers
  • Views 2455 views
  • Users 0 members are here
  • v-usb
  • usb
  • Design
  • attiny
  • arduino
  • vusb
Related

Can someone explain how this V-USB circuit works?

e14 Contributor
e14 Contributor over 12 years ago

Hi everyone,

 

http://www.practicalarduino.com/pics/virtual-usb-keyboard-schematic.jpg

I'm attempting to learn how to communicate with Atmel chips such as the Attiny85 without having to use a serial-to-USB converter. I'm fairly new to electronics circuit design, and I am having trouble understanding what role the zener diodes and resistors have in the communication between the 5V MCU and USB. If you can, please explain why certain resistances and zener diode ratings are used in this situation(and why zener diodes work and regular diodes don't)

 

Thanks in advance,

Tom

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    D_Hersey over 12 years ago

    The designer would have been better served to split his input resistors and place his Zeners at the taps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to D_Hersey

    Not really !

     

    USB chips vary a little but usually need series resistors between zero and 22 ohms. Splitting these doesn't help much - 100V on the zener and 10ohms from that to the chip still makes a dead chip. A big series R would protect the chip nicely but the USB spec can't be met with much more R than the chip supplier recommends and it won't work at all with much more than 100R. You can see one of many better ways to do it here: http://arduino.cc/en/uploads/Main/arduino-uno-schematic.pdf

    (But you won't easily find the devices they refer to so you would need to poke around to find substitutes.)

     

    I would use one of these, you need a board and it's surface mount but ESD protection doesn't really work any other way so nothing is lost:

     

     

    STMICROELECTRONICS - USBLC6-2P6 - DIODE ARRAY, TVS, USB2

     

     

    STMICROELECTRONICSUSBLC6-2P6
    Image is for illustrative purposes only.
    Please refer to product description

     

    Manufacturer:
    STMICROELECTRONICS
    Order Code:
    1295310
    Manufacturer Part No:
    USBLC6-2P6

     

    Technical Data Sheet (219.00KB) EN
    Technical Data Sheet (219.00KB) EN

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 12 years ago in reply to D_Hersey

    Not really !

     

    USB chips vary a little but usually need series resistors between zero and 22 ohms. Splitting these doesn't help much - 100V on the zener and 10ohms from that to the chip still makes a dead chip. A big series R would protect the chip nicely but the USB spec can't be met with much more R than the chip supplier recommends and it won't work at all with much more than 100R. You can see one of many better ways to do it here: http://arduino.cc/en/uploads/Main/arduino-uno-schematic.pdf

    (But you won't easily find the devices they refer to so you would need to poke around to find substitutes.)

     

    I would use one of these, you need a board and it's surface mount but ESD protection doesn't really work any other way so nothing is lost:

     

     

    STMICROELECTRONICS - USBLC6-2P6 - DIODE ARRAY, TVS, USB2

     

     

    STMICROELECTRONICSUSBLC6-2P6
    Image is for illustrative purposes only.
    Please refer to product description

     

    Manufacturer:
    STMICROELECTRONICS
    Order Code:
    1295310
    Manufacturer Part No:
    USBLC6-2P6

     

    Technical Data Sheet (219.00KB) EN
    Technical Data Sheet (219.00KB) EN

     

    MK