Arduino
  • Products
  • More
Arduino
Arduino Forum Cheap, Low Power, Low Cost - 2.4Ghz Wireless Mote (~10$) based on Arduino Friendly nRF24l01
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 419 subscribers
  • Views 905 views
  • Users 0 members are here
  • msp430
  • nrf24l01
  • ti_msp430™
Related

Cheap, Low Power, Low Cost - 2.4Ghz Wireless Mote (~10$) based on Arduino Friendly nRF24l01

gsgill112
gsgill112 over 12 years ago

Hi Friends,

 

I have been thinking of wireless nodes for a while now and came up with the cheapest ever fully sustained

Features,  wireless node :

 

Features....

---------- 2.4GHz (TransReciever) Radio (nRF24L01+ Radio)

---------------------- 32 Bytes of Payload

---------------------- Upto 2MBps Data Rate (~1.76 over AIR)

---------------------- CRC so Accurate

----------------------  ~100 Meters of Range

----------------------  Can connect upto 6 Motes talking to Base Mote parallely

----------------------  Capable of Tree / Star Topology for Network Forming

----------------------  Low Power [Approx 12mA in Rx Mode and ~20mA]

 

--------- MSP430G2553 MCU

---------------------- 16MHz, 16-Bit, 16KB Flash

---------------------- 2-Timers, and much more ..

image

 

Please tell me what do you guys think !!

 

A Simple Scenario:

 

              node2         <=

node1         <=           <=            <=          nRF24<--->node4 <--->Wifi Interface        <=               <=                 <=     You Controlling through Wifi image

                        node3  <=

 

conceder this scenario, we can gather all the data from nodes or/ give a command to nodes using our WIFI on laptop/Etc. , and let node4 control all the other nodes , hence forming a network !!

 

 

P.S. :::::: Sorry for reposting this , I am a new user to The Knode

  • Sign in to reply
  • Cancel
Parents
  • vish
    vish over 12 years ago

    Hi Gurinder,

    I'm trying to find (nRF24L01+ Radio) online, but can't find it at the price range you are mentioning. Whatever I found in online stores is well above the price you are mentioning. Could you please post any links/sites from where I can get this( at low cost ).

    And could you also mention what are the exact parts required. I have a MSP430G2. Is nRF24L01+Radio a single module or do I have to buy them separately?

     

    Thanks ahead,

    vish

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to vish

    Low power at US$2.45 each

    http://yourduino.com/sunshop2/index.php?l=product_detail&p=188

     

    Terry also has higher power versions

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to mcb1

    typically the NRF24L01 have a limited range being at 2.5Ghz, they have very optomistic claims in their documents

     

    the NRF905 being a sub Ghz model should give you much better range and of course there is the TI versions based on the CC1100 series radios

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to Robert Peter Oakes

    Peter

    edit after finding the datasheet.

    By chance is that in the 900Mhz range.

     

    I see that you can change them to 433 MHz making them legal here in NZ (why use the 905 name ... what about ">1GHz" )

    I'll have to see who sells them and take them for a spin.

     

     

    Out of interest I pledged for these  http://www.rfdigital.com/wp-content/uploads/2014/03/rfduino.datasheet.pdf  and they arrived during a busy time, but looking at them they use FCC approved low power bluetooth.

     

     

    Thanks for that

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to mcb1

    they look very nice but at what point does too small come into play

     

    I'm all for these devices being available for evaluation and experimentation but when you finally want to build  a real project and include a few different modules all using the same controller, it is a pain to connect them all and which one to go for, there are way to many different connector specifications .

     

    Don't get me wrong, those modules look great, just when you have a bunch to put together, it becomes a problem, I see so many modules with not easy way of mounting them in a case or on a chassis. There is definitely a lack of connector standards that needs to be addressed ?

     

    shields, capes, PI Crusts, you name it, there is no consistent standard on how to connect that SPI device or the I2C device... Wow i can rant

     

    anyway you get my point and as useual we TM members digress from time to time... Ah well image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to mcb1

    they look very nice but at what point does too small come into play

     

    I'm all for these devices being available for evaluation and experimentation but when you finally want to build  a real project and include a few different modules all using the same controller, it is a pain to connect them all and which one to go for, there are way to many different connector specifications .

     

    Don't get me wrong, those modules look great, just when you have a bunch to put together, it becomes a problem, I see so many modules with not easy way of mounting them in a case or on a chassis. There is definitely a lack of connector standards that needs to be addressed ?

     

    shields, capes, PI Crusts, you name it, there is no consistent standard on how to connect that SPI device or the I2C device... Wow i can rant

     

    anyway you get my point and as useual we TM members digress from time to time... Ah well image