Arduino
  • Products
  • More
Arduino
Arduino Forum Wearable Tech - What's next?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 420 subscribers
  • Views 2289 views
  • Users 0 members are here
Related

Wearable Tech - What's next?

morgaine
morgaine over 12 years ago

I'll elaborate a little on the points raised about combining art with technology, specifically about assessment.

 

Although art/craft and sci/eng can yield very interesting results in combination, it's worth pointing out that they are so dissimilar in nature that they are almost entirely unrelated to each other, and so the perceived properties of the end result stem not from their combination but from each individually.  Let me explain.

 

The perceived merit of an item of art lies completely in the eye of the beholder --- one and the same piece of art can be seen as wonderful by one person and dreadful by another, and neither of them is right nor wrong.  Not even the opinion of the world's top expert in fine arts will make it good when another person's judgment finds it bad.  In other words, appreciation of the artistic qualities of an item is completely subjective.  (Note that many items of art have functional aspects as well --- that's separate, and dealt with now.)

 

The merit of a technological mechanism is entirely functional --- it either does the job for which it was designed successfully or poorly or not at all, and this assessment is measurable and objective.  Of course, different people may have different requirements and they sometimes shift the goalposts when assessing whether desired functionality has been met, but a mismatch between the assessor's requirements and the design requirements is no fault of the device or the technology.  Assessment of the item's merit measured against its own design goals is always objective.  (Note that many products of technology have artistic aspects as well, but those are only by coincidence related to the function and should be assessed on their own merits.)

 

This essential difference between the artistic merit and the technological merit of an item that combines both is so stark that they don't really affect each other --- the technical term for this is orthogonality.  Sometimes people think that some particular functionality is ugly or beautiful, but this is actually wrong because it confuses two issues, the function and the implementation of that function.  The same functionality could in principle be implemented in many different ways, and it could even be hidden entirely, so ugliness or beauty cannot be a subjective attribute of the functionality whose degree of success can be determined objectively.  Instead, the chosen implementation of the function usually has a physical aspect, and it is this physical aspect that may attract subjective merit or criticism.  Functionality actually has no artistic dimension at all.  (If we say that something "operates beautifully", that's really just a metaphor.)

 

The latter statement needs some elaboration, because scientists, engineers and technologists in general often use terms that are undoubtedly subjective when assessing a technical design:  for example, we often say that a good design is elegant, or efficient, or minimalist, and we might say that a bad design is convoluted, or inefficient, or over-engineered, and so on.  Doesn't this mean that the merits of our technology are subjective as well?  Not really, because again two things are being conflated, the functional merit (how closely it meets its design requirements) and how well it fares on secondary figures of merit that are not design requirements, eg. our individual concept of elegance.  (Requirements have to be measurable, otherwise compliance cannot be determined).  As was mentioned earlier, changing the goalposts does not make sense in engineering assessment.

 

This finally brings me back to my opening point about how to assess an item that combines elements of art and technology.  When adding a technological element like LEDs to a wearable, it's tempting to think that LEDs add artistic value.  They don't, at least not directly.  They add light, and it is the light that may or may not provide artistic value, and this same light could be generated by other means.  The LEDs can be assigned nothing more than a functional figure of merit based on whether they are working or not, whether they are bright enough or not, whether they are the desired colour, whether they use too much current, and so on --- and all of these properties appear on the datasheet.  They are objective, not subjective.  If you chose particular LEDs but you didn't find the end result artistically pleasing, this is not a failure of the LEDs --- functionally the technology is perfect (unless they're faulty) --- instead, it's a failure of your choice of light for your design.  Of course, somebody else could express surprise at your disappointment, because to them it looks beautiful.  The artistic merit is not a functional property of the LEDs. image

 

In summary, I'll answer Leslie's point #2 in this way:  if you've combined art with technology then you have inherently added function, so it can never be not functional (unless it's faulty of course).  The function may be nothing more than to add an effect for artistic purposes (for example light), but you can't sensibly apply artistic judgements to the function.  If the light that is produced is exactly that intended by the design then it's functionally perfect, even if the end result is artistically ugly as sin to every living being on the planet. image  Even when combined, art and technology live in inherently different spaces, and what they each contribute cannot be judged by a single measuring stick.

 

Morgaine.

 

 

Addendum:  The above has the rather curious consequence that despite combining them together in the same item, artistic and technological design are necessarily separate because the goal of one is a desired value judgment and the goal of the other is correct functional operation.  The mind can try to maneuver them both towards a common goal, but they're essentially different occupations.

  • Sign in to reply
  • Cancel

Top Replies

  • morgaine
    morgaine over 12 years ago in reply to johnbeetem +1
    For the purposes of this discussion, canaries and humans can be considered identical in their use of acoustic perception to process incoming sound waves. (Not surprising, since all life on Earth has extremely…
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine +1
    Morgaine Dinova wrote: A species on a different planet could in principle look at some utter rats nest of code that I would never dare release because it is revolting even to me and releasing it publicly…
  • zengirl2
    zengirl2 over 12 years ago in reply to fustini +1
    I really like this and it reminds me of the work of Hi-Low Tech at MIT. I see that Jesse also follows the work of Hannah Perner. She is one of my faves working with soft circuits and I met her two year…
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    Morgaine Dinova wrote:

     

    Although art/craft and sci/eng can yield very interesting results in combination, it's worth pointing out that they are so dissimilar in nature that they are almost entirely unrelated to each other, and so the perceived properties of the end result stem not from their combination but from each individually.

    I don't agree with that.  I see art and engineering working in harmony, with outstanding engineering producing the same aesthetic thrill as "pure" art.

     

    Exhibit A:  The works of architect Antoni Gaudi combine beautiful art along with sound structural engineering.  Some of his works are so fanciful that it's amazing that they stand, yet if you look at the structural engineer underneath it is completely sound and meshes perfectly with the art.  In contrast, Frank Lloyd Wright's buildings often have structural problems in spite of their beauty.

     

    Exhibit B:  I once challenged myself to route a rather dense board on two signal layers.  The primary components on the board were an FPGA in PQFP-208 package and a CPLD in a TQ-100, plus some SOIC bus switches to protect 3.3V FPGA I/Os from 5V circuits.  Through very careful pin assignment of the FPGA and CPLD, I was able to do it in two signal layers and the aethetics of the board are quite beautiful, with wonderful parallel rivers flowing across the board and between SOIC pins instead of the "swiss cheese" of a many-layered board.

     

    Exhibit C:  The Eiffel Tower.

     

    Exhibit D:  Myriad steel structures of the 19th Century and early 20th Century before the suits in accounting decided buildings had to be purely functional and there was no room for art.

     

    In my own work, I find that my hardware and software designs that are aesthetically pleasing function better, and that if the design starts to look "ugly" then there's got to be a better way to do it -- and there usually is.

     

    Some of this is probably from my upbringing.  I was a born engineer, with the engineer gene inherited from my grandfather.  However, my parents are both academics: Art History and English Lit.  So I've ended up as a generalist in an age of specialists.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I don't agree with that.  I see art and engineering working in harmony, with outstanding engineering producing the same aesthetic thrill as "pure" art.

     

    This "harmony" of which you speak, please define it for me in scientific/engineering/mathematical terms --- I bet you can't, and if you can't then it doesn't belong there.  The reason you can't is because it's not a figure of merit from the scientific/engineering/mathematical world at all, but from the world of human appreciation, a subjective value judgment.  That subjective value judgement is completely separate from the objective functional property that the human examines to return that value judgment.

     

    In other words you've conflated your artistic sensibilities with your sci/eng/math observations and believe them to be a single step, when they're not.  With some slightly deeper analysis, those two things can be disentangled.  I'll try below.

     

    (I'm afraid I don't know anything about architecture, but we share a love and some knowledge of music, so let's use that as a subject domain for some analysis and examples.)

     

    In music, a set of pure tones are often said to be in harmony or disharmony --- this is the foundation upon which the entire edifice of the study and performance of music is based.  It's relatively simple so it gives us a good basis for analysis.  Pure tones are sounds containing single frequencies devoid of any accompanying harmonics that give a sound timbre or "color" --- the phrase more or less contains its own definition, ie. "no overtones".  A pure tone has only three physical properties, its frequency ("pitch"), its amplitude ("volume" or "intensity"), and its phase --- just for simplicity I'll leave the 2nd and 3rd ones out of the discussion initially, but they're listed in case we need them later.

     

    So. let's start by talking about frequency and about pitch.  In the paragraph above I've placed the two words next to each other and they're presented as if they were synonyms, but they're not.  Frequency is an objectively measurable physical property of a pure tone, whereas pitch is a perceptual property determined by the very complex human auditory system comprising ears, neural pathways and our brains.  (Not only human of course, but let's stick to humans here.)  Pitch is studied in psychoacoustics.  Perceptual properties like pitch are always subjective, and pitch is only a sensation, not a physical property of a pure tone.  Fortunately most people perceive pitch very similarly, although there are anomalies just as we find in the perception of light (colour blindness and related pathologies are very well known).  Because the perceived pitch so commonly corresponds directly to the objectively measured frequency, it is extremely usual to conflate them together and treat them as one, but this is incorrect.  We know it's incorrect, yet we commonly use these two words as synonyms simply as a shortcut.  Life is full of shortcuts, and very useful they are to us, but one must always be aware that a shortcut is a shortcut and not treat it as anything stronger like equivalence.

     

    So, we've already left the objective domain when we talk about pitch, but it's about to get worse.  We can't talk about harmony in the context of a single pure tone, we need a set of two or more of them taken together in order to discuss whether they harmonize or not.  So, let's use a set of perfect sinusoidal frequency generators and perfect amps and perfect speakers to generate two or more pure tones in the lab for analysis of whether they harmonize.  (I'll stick to just two pure tones here, but the same applies to any number greater than one, although it gets horribly complex with a large set.)

     

    "But wait", you cry, "don't leave the objective lab just yet, we can tell if they harmonize just from their frequencies!".  Not so fast, cowboy, you're conflating the expectation of harmony or disharmony as perceived by most humans with what is actually happening in the physics.  Nature or reality doesn't know about harmony.  Two frequencies will "beat" when combined if their frequencies are not identical nor integer multiples of a fundamental, but all beating frequencies are the same to nature --- she doesn't consider some as "harmonious" and some as "disharmonious".  With larger sets of pure tones, she doesn't consider certain combinations of beating frequencies as harmonious chords and others as horrible dischordant sounds --- those are human value judgments, and they're subjective.  Beating is a completely objective physical function and can be measured without involving the naturally subjective human perceptions and value judgments.  So no, we can't discuss harmony without bringing in the human angle.  Ratios of frequencies are just another of those very useful shortcuts that allow us to predict expected perceptions in the subjective world, nothing more.

     

    The subjective rabbit hole opened up by examining harmony goes very deep indeed.  Consonance and dissonance are related subjective properties used as metrics in musical sound perception, and they are so subjective that they are affected strongly by cultural groupings and history, and even by prior acquaintance or exposure to the sound.  This rabbit hole goes far, far outside the realm of objective reality.

     

    So to recap, when art is combined with technology, any perceived artistic merit or demerit in the technology is not an assessment of its objective functional properties, but a subsequent subjective assessment of its side effects at most. Our perceptions are side effects of the operation of the technological element in art even when the whole purpose of the technology is to create those perceptions, and it is those perceptions that result in our labeling the result as artful or not.  The function itself is not artful, and it makes no sense to describe it in those terms because those terms are not part of the objective domain in which the function is defined.  The function is either operating correctly or it is not, or somewhere in between, and that is all you can say about it in the objective world.  You have to leave that world to make a value judgment about artistic merit.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Nature or reality doesn't know about harmony.  Two frequencies will "beat" when combined if their frequencies are not identical nor integer multiples of a fundamental, but all beating frequencies are the same to nature --- she doesn't consider some as "harmonious" and some as "disharmonious".  With larger sets of pure tones, she doesn't consider certain combinations of beating frequencies as harmonious chords and others as horrible dischordant sounds --- those are human value judgments, and they're subjective.

     

    I have a friend who is a historic keyboard specialist, who is the source for most of what I know about historic tunings.  At one time she had a very spirited canary who helped her tune harpsichords and pianos.  If she had the tuning just right, Wolfie would trill joyfully (or at least in a manner suggestive of joy to us mere humans).  Sure, she could also use an Accu-Tuner, but Wolfie was just as good.

     

    Regarding nature and reality: I guess a good question is whether humans are part of nature and/or reality, or whether they are unwelcome guests or outright intruders [1].  I suspect the answer to that question is that it depends on the human.  I like to think of myself as part of nature as evidenced by how much I abhor vacuuming [2].

     

    [1] Adapted from Maj. Giles Flack's sermon in Privates on Parade.

    [2] AKA "hoovering".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    John Beetem wrote:

     

    I don't agree with that.  I see art and engineering working in harmony, with outstanding engineering producing the same aesthetic thrill as "pure" art.

     

    This "harmony" of which you speak, please define it for me in scientific/engineering/mathematical terms --- I bet you can't, and if you can't then it doesn't belong there.  The reason you can't is because it's not a figure of merit from the scientific/engineering/mathematical world at all, but from the world of human appreciation, a subjective value judgment.

     

    Wiktionary defines harmony as "(1) Agreement or accord, (2) a pleasing combination of elements" and a number of music-specific definitions.  When I look at the Eiffel Tower, I see both the simplistic beauty of the overall lines and the intricacies of the steel lattices that create curves from straight steel girders.  I also see how the structure takes the mechanical stresses of a gigantic tower and distributes them downwards and outwards to keep the tower strong and stable even in high winds.  The Eiffel Tower is "a pleasing combination of elements" to me as a human -- though many considered it a monstrosity when it was first built.  But it's also pleasing to the forces of nature that it works with to last for over 100 years.  I won't say the tower "exploits" these forces, because it's nature that's in charge here -- the Tower works in accord with the forces.  Engineering is the art of understanding these forces and using their nature to build something useful.  And if you use them particularly well, the result often is aesthetically pleasing -- at least to this engineer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    John Beetem wrote:

     

    I don't agree with that.  I see art and engineering working in harmony, with outstanding engineering producing the same aesthetic thrill as "pure" art.

     

    This "harmony" of which you speak, please define it for me in scientific/engineering/mathematical terms --- I bet you can't, and if you can't then it doesn't belong there.  The reason you can't is because it's not a figure of merit from the scientific/engineering/mathematical world at all, but from the world of human appreciation, a subjective value judgment.

     

    Wiktionary defines harmony as "(1) Agreement or accord, (2) a pleasing combination of elements" and a number of music-specific definitions.  When I look at the Eiffel Tower, I see both the simplistic beauty of the overall lines and the intricacies of the steel lattices that create curves from straight steel girders.  I also see how the structure takes the mechanical stresses of a gigantic tower and distributes them downwards and outwards to keep the tower strong and stable even in high winds.  The Eiffel Tower is "a pleasing combination of elements" to me as a human -- though many considered it a monstrosity when it was first built.  But it's also pleasing to the forces of nature that it works with to last for over 100 years.  I won't say the tower "exploits" these forces, because it's nature that's in charge here -- the Tower works in accord with the forces.  Engineering is the art of understanding these forces and using their nature to build something useful.  And if you use them particularly well, the result often is aesthetically pleasing -- at least to this engineer.