Arduino Forum Hi how to convert analogy signal to digital signal in arduino
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
  • Replies 11 replies
  • Subscribers 404 subscribers
  • Views 1614 views
  • Users 0 members are here
Related

Hi how to convert analogy signal to digital signal in arduino

Former Member
Former Member over 11 years ago

Hi! Can some one help me with Arduino codes for converting analog signal to digital signal.

There four input analog signal wishing to convert each them to digital signal.

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 11 years ago

    what is your required sampling rate and resolution, also do you know the signal voltage range of the analog input is?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • heliosoph
    heliosoph over 11 years ago in reply to Former Member

    If you need more information about the analog inputs of the arduino look at:

     

    http://arduino.cc/en/Tutorial/AnalogInputPins

     

    The analogRead instruction is described here:

     

    http://arduino.cc/en/Reference/AnalogRead

     

    When you have your arduino IDE installed look in the examples, analog section

     

    heliosoph

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to heliosoph

    Thanx alot I have tried to code but I when I try to run my codes I encounter an error,so can any one help me to solve this issue.

     

     

    int inputPins[] = {2,3,4,5}; // create an array of pins for  inputs

    int lcdPins[] = {0,1,2,3,4,5,6,7}; // create array of output pins for LEDs

    void setup()

    {

    for(int index = 0; index < 3; index++)

    {

    pinMode(inputPins[index], INPUT); // declare  inputpins

    }

    }

    void loop(){

    for(int index = 0; index < 4; index++)

    {

    analogRead(inputPins[index]); // read input val

    }

     

    float val0=analogRead(inputPins[0]);

    float val1=analogRead(inputPins[1]);

    float val2=analogRead(inputPins[2]);

    float val3=analogRead(inputPins[3]);

     

    if(val0 >=0.2){

      digitalWrite( val0,HIGH); 

    }

     

    else if (val1>= 1.5){

       digitalWrite( val1,HIGH); 

    }

    else if (val2>val 3){

      digitalWrite(val2,HIGH);

    }

     

    else

    digitalWrite( val0,LOW );

    digitalWrite( val1,LOW );

    digitalWrite( val2,LOW );

     

    if (val0==LOW && val1==LOW && val2==LOW){

      Serial.println("Blood group O-");

    }

    else if (val0==LOW && val1==LOW && val2==HIGH){

      Serial.println("Blood group O+");

    }

    else if (val0==LOW && val1==HIGH && val2==LOW){

      Serial.println("Blood group B- ");

    }

    else if (val0==LOW && val1==HIGH && val2==HIGH){

      Serial.println("Blood group B+");

    }

    else if (val0==HIGH && val1==LOW && val2==LOW){

      Serial.println("Blood group A-");

      }

     else if (val0==HIGH && val1==LOW && val2==HIGH){

      Serial.println("Blood group A+");

    }

    else if (val0==HIGH && val1==HIGH && val2==LOW){

      Serial.println("Blood group AB-");

    }

    else if (val0==HIGH && val1==HIGH && val2==HIGH){

      Serial.println("Blood group AB+");

    }

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    Hello Francis,

     

    you have only a little typo in your code:

     

    else if (val2>val 3){
      digitalWrite(val2,HIGH);
    }

     

    The space in "val 3" must be deleted:

     

    else if (val2>val3){
      digitalWrite(val2,HIGH);
    }

     

    This should work. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to Former Member

    Thanx I have runned codes but it only displays the single blood group  o- with reference to my circuit below when I try to alternate for swichtch states.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • heliosoph
    heliosoph over 11 years ago in reply to Former Member

    I think you have a mess with your variables:

      digitalWrite( val0,HIGH);

    val is your variable where you store your values from analogRead. In digitalWrite() you have to use a (digital) pin number. The pin you want to set to high.

     

    Elektrix

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to heliosoph

    With this code still no change observed

     

    #include <LiquidCrystal.h>

     

     

     

     

    int inputPins[] = {2,3,4,5}; // create an array of pins for  inputs

    int lcdPins[] = {12,11,5,4,3,2}; // create array of output pins

    LiquidCrystal lcd(12,11,5,4,3,2);

    void setup()

    {

    for(int index = 0; index < 3; index++)

    {

    pinMode(inputPins[index], INPUT); // declare  inputpins

    }

    }

    void loop(){

    for(int index = 0; index < 4; index++)

    {

    analogRead(inputPins[index]); // read input val

    }

    float A0=analogRead(inputPins[0]);

    float A1=analogRead(inputPins[1]);

    float A2=analogRead(inputPins[2]);

    float A3=analogRead(inputPins[3]);

    if(A0 >=0.2){

      digitalWrite( A0,HIGH);

    }

     

     

    else if (A1>= 1.5){

       digitalWrite( A1,HIGH);

    }

    else if (A2>A3){

      digitalWrite(A2,HIGH);

    }

     

     

    else

    digitalWrite( A0,LOW );

    digitalWrite( A1,LOW );

    digitalWrite( A2,LOW );

     

     

    if (A0==LOW && A1==LOW && A2==LOW){

    lcd.println("Blood group O-");

    }

    else if (A0==LOW && A1==LOW && A1==HIGH){

      lcd.println("Blood group O+");

    }

    else if (A0==LOW && A1==HIGH && A2==LOW){

      lcd.println("Blood group B- ");

    }

    else if (A0==LOW && A1==HIGH && A2==HIGH){

      lcd.println("Blood group B+");

    }

    else if (A0==HIGH && A1==LOW && A2==LOW){

      lcd.println("Blood group A-");

      }

    else if (A0==HIGH && A1==LOW && A2==HIGH){

      lcd.println("Blood group A+");

    }

    else if (A0==HIGH && A1==HIGH && A2==LOW){

      lcd.println("Blood group AB-");

    }

    else if (A0==HIGH && A1==HIGH && A2==HIGH){

      lcd.println("Blood group AB+");

    }

    else

    lcd.println("device error");

    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago in reply to heliosoph

    With this code still no change observed

     

    #include <LiquidCrystal.h>

     

     

     

     

    int inputPins[] = {2,3,4,5}; // create an array of pins for  inputs

    int lcdPins[] = {12,11,5,4,3,2}; // create array of output pins

    LiquidCrystal lcd(12,11,5,4,3,2);

    void setup()

    {

    for(int index = 0; index < 3; index++)

    {

    pinMode(inputPins[index], INPUT); // declare  inputpins

    }

    }

    void loop(){

    for(int index = 0; index < 4; index++)

    {

    analogRead(inputPins[index]); // read input val

    }

    float A0=analogRead(inputPins[0]);

    float A1=analogRead(inputPins[1]);

    float A2=analogRead(inputPins[2]);

    float A3=analogRead(inputPins[3]);

    if(A0 >=0.2){

      digitalWrite( A0,HIGH);

    }

     

     

    else if (A1>= 1.5){

       digitalWrite( A1,HIGH);

    }

    else if (A2>A3){

      digitalWrite(A2,HIGH);

    }

     

     

    else

    digitalWrite( A0,LOW );

    digitalWrite( A1,LOW );

    digitalWrite( A2,LOW );

     

     

    if (A0==LOW && A1==LOW && A2==LOW){

    lcd.println("Blood group O-");

    }

    else if (A0==LOW && A1==LOW && A1==HIGH){

      lcd.println("Blood group O+");

    }

    else if (A0==LOW && A1==HIGH && A2==LOW){

      lcd.println("Blood group B- ");

    }

    else if (A0==LOW && A1==HIGH && A2==HIGH){

      lcd.println("Blood group B+");

    }

    else if (A0==HIGH && A1==LOW && A2==LOW){

      lcd.println("Blood group A-");

      }

    else if (A0==HIGH && A1==LOW && A2==HIGH){

      lcd.println("Blood group A+");

    }

    else if (A0==HIGH && A1==HIGH && A2==LOW){

      lcd.println("Blood group AB-");

    }

    else if (A0==HIGH && A1==HIGH && A2==HIGH){

      lcd.println("Blood group AB+");

    }

    else

    lcd.println("device error");

    }