Arduino
  • Products
  • More
Arduino
Arduino Forum LCD Problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 419 subscribers
  • Views 2248 views
  • Users 0 members are here
  • lcd
  • arduino
Related

LCD Problem

e14 Contributor
e14 Contributor over 12 years ago

Hi I have a problem with the LCD. I have everything that it is shown in jeremy blums book about displaying a text in lcd but still have problem. I see nothing. Can anyone help me?

The thing that I used is 10K potentiometer or not?

Fullscreen contentimage_76500.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    there are two threads almost the same, please read my post on the other thread and let us know if it resolved your problem. http://www.element14.com/community/thread/32268/l/arduino-lcd-help

     

    it looks like you may have a similar issue, also try the software and wiring that is used on the other thread, it may be the same but just in case... I verified that setup myself and it does work

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    Hi and thank you for replying. I solve my problem but I want to ask you something else. My LCD is working but sometimes it displays thing that i hadn't written and so on. I want to inform you that I didnt yet soldered the LCD. Do you think that this is the problem? TY again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago in reply to e14 Contributor

    It could be bad connection on the bread board for sure, especially if you have been plugging in large wire components in the past and are now using smaller wires. another possibility is that some displays have different character sets in them, this would only affect characters outside of the normal a-z, 0-9 though. so if your re-running the same test again and again, with different output sometimes then I would suspect the wiring to be the cause.

     

    btw, what was the cause of your previous problem, you did not say

     

    glad your up and running btw.

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    I think that the pins wasnt in touch well. So i moved it a lot of time and then realized that something appears. But now the problem is; that sometimes it appears different letter instead of the required. So i need to move it a lof of time. Once more, do you think that its because i didnt soldered it or not? And what do you suggest me? You can also show it to me with pictures. Thanks once again for helping me

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    The photo appears to show that the header is not soldered to the LCD.

    This is sure to cause problems.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mcb1

    Yes, its not soldered. I thought that it would worke like that too. So, do you think that this causes the problem?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    This is sure to cause problems.

    As I said above.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 12 years ago in reply to e14 Contributor

    You definitely need to solder that header onto the LCD. Remove the header from the breadboard before you do. There has to be a good connection between the pad on the LCD board, and the header pin, so soldering it is the best and cheapest choice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelwylie

    Thank you very much. I thought it has no problem since the pins are connected to the LCD image.

    Thanks again

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelwylie
    michaelwylie over 12 years ago in reply to e14 Contributor

    The pins are connected to the LCD? Is it soldered on the backside and we just can't see?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelwylie
    michaelwylie over 12 years ago in reply to e14 Contributor

    The pins are connected to the LCD? Is it soldered on the backside and we just can't see?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelwylie

    No, no. Nothing is soldered. What I mean is that I thought it has no problem since the header is connected to the LCD. By the way I am programmer and I almost know nothing about electronics. So, I am sorry for my silly questions. Last thing, do you have the time to explain me why soldering is important?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    The connection is not made until it soldered.

    At the moment its a very poor and intermittant joint between the header pins and the lcd.

     

    The breadboard has contacts that 'grip' the pin and therefore make contact.

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mcb1

    Umm. I see. Thats was really informative.

    thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    If you wish to avoid having to solder there are several alternatives.

    There is an LCD shield available that includes some pushbuttons and is designed to go onto the Arduino.

     

    There is also some I2C LCD's and I use these. http://yourduino.com/sunshop2/index.php?l=product_detail&p=331

    A 4 pin lead is all you need to connect since they have a small extra board that converts the I2c data to the display.

     

    Sadly element14 don't carry them and it would be very useful to their range.

     

    Mark