Arduino
  • Products
  • More
Arduino
Arduino Forum Hi to everyone, i'm XarlyX And I Need Help With A LCD
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 419 subscribers
  • Views 1050 views
  • Users 0 members are here
  • lcd
  • printer
  • lexmark
  • arduino
Related

Hi to everyone, i'm XarlyX And I Need Help With A LCD

xarlyx
xarlyx over 12 years ago

Hi.

 

I'm new to this comunity, i hope to fit well here.

 

The reason i sing up to this comunity is that:

 

Few weeks ago i unscrewed a Lexmark x3350 printer for salvaging lot of cool stuff,like a 10-pin LCD display, found at the control pannel of the printer.

i took the PCB and disolder the screen carefully. behind the LCD, in the PCB the're wasn't any IC or SMD, only a few resistors so i thank: Could i use it with my Arduino UNO?.

 

I searched in the internet but i havn't found any specs or any class of information, so... Could you help me please? at the moment i only want to know how it works and the pinout for printing at the screen a kind of "Hello World", only that. so Thanks so much for reading my first post

  • Sign in to reply
  • Cancel

Top Replies

  • michaelwylie
    michaelwylie over 12 years ago in reply to xarlyx +1
    The numbers we are interested in are likely under the black plastic. Anyway to get in there without hurting the LCD?
Parents
  • dougw
    dougw over 12 years ago

    Hi Xarly,

    I have not seen a display that looks like this, but if you want some wild speculation to check out - the ubiquitous Hitachi LCD controller (HD44780) can be connected using 10 pins, so there is a chance this popular controller is buried in there using chip-on-glass or glob top methods. (With only 10 pins it must have a controller chip in it somewhere.)

    Typical signals in such an interface would be:

     

    LCD Pin Connect to
    1 (VSS) GND Arduino pin*
    2 (VDD) + 5v Arduino pin
    3 (contrast) Resistor or potentiometer to GND Arduino pin*
    4 RS Arduino pin 12
    5 R/W Arduino pin 11
    6 Enable Arduino pin 10
    7 (Data 4) Arduino pin 5
    8 (Data 5) Arduino pin 4
    9 (Data 6) Arduino pin 3
    10 (Data 7) Arduino pin 2

     

    You can look up how to connect a typical display to an arduino, but keep in mind this speculation is potentially completely wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • xarlyx
    xarlyx over 12 years ago in reply to dougw

    To @Douglas Wong:

     

    Hi douglas, thanks for the pinout of the HITACHI controller, in a minute i will connect it to my Arduino so... i will tell you later, the "sketch" of the lcd is included on the IDE of Arduino for Windows no?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • xarlyx
    xarlyx over 12 years ago in reply to dougw

    To @Douglas Wong:

     

    Hi douglas, thanks for the pinout of the HITACHI controller, in a minute i will connect it to my Arduino so... i will tell you later, the "sketch" of the lcd is included on the IDE of Arduino for Windows no?