Arduino
  • Products
  • More
Arduino
Arduino Forum Vote in three minutes!
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 419 subscribers
  • Views 1415 views
  • Users 0 members are here
Related

Vote in three minutes!

e14 Contributor
e14 Contributor over 12 years ago

No more long queues at polling stations. I am doing a project on voting using a cell phone with a cell phone based voting machine using micro controller AT89S51. I am stuck at writing a code for this project.

  • Sign in to reply
  • Cancel

Top Replies

  • sqkybeaver
    sqkybeaver over 12 years ago in reply to Robert Peter Oakes +1
    if you must use 8051 you should look at this C8051F12x/3x 8-bit Microcontroller (MCU) | Silicon Labs
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 12 years ago

    My initial question is why this micro-controller

     

    It is an industry standard sure but very limited for something like your attempting, more IO than you need and probably way less Program and Ram space than you will need

     

    I would suggest an Arduino UNO or higher Arduino or if you making a custom board, an ATMEGA 328 (Uno can be the development platform, then unplug the chip into your own custom board if needed

     

    You can use the free IDE/Compiler and it is programed in standard C. You should still be able to interface to all your peripherals without an issue and there are loads of people in the community who will be able to help

     

    there are also plenty of shields to provide internet access and other functionality with ready made libraries for your consumption

     

    If your new at this, perhaps you should consider this walk before you run approach and it has the FLASH memory for program, EEPROM for storing variables and SRAM for the run time way in excess of the 8051 based micro you mention

     

    328 has

    32K FLASH Program Space

    2K SRAM

    1K eeprom

     

    at89s51

    4K FLASH (Program Space)

    128bytes ram

    no eeprom

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    ATMEGA 328 makes work easier now, i like it. Thanks for insight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Robert Peter Oakes

    ATMEGA 328 makes work easier now, i like it. Thanks for insight.